2013-05-31 11:55 PM
hi
I have a problem
with jtag tck pin on my board.When
I touch
it with
myfinger
the st-linkWorks properly
& connect to stm32f417 but if i remove my finger from this pin the st-link not connect to my mcu.i pull-down tck pin with 10k to gnd.Also, when
i connect my board's gnd to pc casethis
problem
can be
solved
.What is
the problem?why tck pin is sensitive to the touch of my finger
???2013-06-01 4:39 AM
Sounds like some supply connectivity issues, perhaps a schematic and diagram of the connections made would be illustrative.
How is the board powered? How are grounds on the ST-Link connected to your board.2013-06-01 9:45 PM
i convert (2*10 )jtag connector to header (1*7) & only use
NRST TDI TDO TCK TMS GND VDD on my board.also don't use JTAG TRST & pull-up it on my board