STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Card detect and Dat 3 on SDIO ?

Posted on April 10, 2014 at 12:36Guys, Do I need to use Card detect ? (CD) because it's joined together on my connector...and in the code it's separated as two pins ? Any ideas ? thanks

0690X00000602ssQAA.jpg 0690X00000602jmQAA.jpg

stm32f4 usart max speed

Posted on April 02, 2014 at 11:26I'm using stm32f407 combined with ftdi232h usb-serial converter. Every byte I call an interrupt and send back the same byte to check. This works fine with baud rate to 115200. I have tried to force best baud rate (th...

UART Comm between stm32f407 and stm32f030 (full duplex)

Posted on March 27, 2014 at 13:23Did any body experience in communicating between two different boards (full duplex) . Please help me with code the controller can be of anything just I need a example for reference. Please help me

sanjib by Associate III
  • 1990 Views
  • 7 replies
  • 0 kudos

[STM32F072] USART2 and USART4 does not work

Posted on April 10, 2014 at 13:50Hello all, I'm recently bought an STM32F072B-DISCO board (based on the STM32F072RBT6) and I'm currently testing it. I'm really surprised to see that some USARTs doesn't work properly ; as mentioned in the errata shee...

louis2 by Associate
  • 1285 Views
  • 3 replies
  • 0 kudos

STM32F205RBT6 - usart1 baud rate 1200

Posted on April 10, 2014 at 14:34I am running STM205RBT6 on 120 Mhz & fpclk = 60Mhz for usart 1.I need to run usart1 on 1200 baud rate.For that I have calculate value of BRR = 0xC350.Is it right??

Data Align Packed Struct

Posted on April 10, 2014 at 14:18I need to be sure that a struct I use has 32-bit alignment. My IDE (IAR) gives a preprocessor directive for this, which I am trying to use. However, the compiler keeps giving me warnings saying that I can't use this ...

jvavra by Associate III
  • 1035 Views
  • 1 replies
  • 0 kudos

IAR Embedded WorkBench IDE for STM32L

Posted on July 18, 2013 at 08:28All,My question is related to IAR Embedded WorkBench IDE 6.50 for STM32L. I think somebody using the IDE can help me to solve the issue or else can direct me to a better place in which I can find Support regarding the...

STM32F2xx HS USB MSD fault on cards over 4GB

Posted on April 09, 2014 at 14:49I have taken the code from the stm3220G - eval board and change the HSE setting to match my hardware. I have also configured the HS port to us the embedded phy. the storage media is a SD card driven via the SDIOThis ...

dcurran2 by Associate II
  • 2032 Views
  • 5 replies
  • 0 kudos

STM32Cube FW USB_Device MSC

Posted on March 27, 2014 at 11:18hi, I have a problem with Application from STM32Cube_FW_F4_V1.1.0. It´s the USB_Device -> MSC_Standalone application. When I build the files with Coocox and download it on my STM3240G-Evalboard, the USB-Device will b...