STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32-Mat TIMx-IRQHandler multiply defined

Posted on June 11, 2014 at 11:53Trying to generate a simple PWM Output using STM32-Mat Timers 1 and 8 work flawlessly, however the other available timers (2,3,4,5) all produce error 6200: TIMx-IRQHandler multiply defined by stm32f4xx.o and PWMTest.o...

marc2 by Associate II
  • 788 Views
  • 0 replies
  • 0 kudos

Lwip stack for Standalone STM32F407VG

Posted on June 06, 2014 at 15:42Hi AlI have referred to  AN3966 (LwIP TCP/IP stack demonstration for STM32F407/STM32F417 microcontrollers) to get LWIP stack for Standalone STM32F407VG. And also i got LWIP stack files from a link http://www.st.com/we...

ecmanja by Associate II
  • 4730 Views
  • 10 replies
  • 0 kudos

Hard fault problem

Posted on June 10, 2014 at 16:34 For several years I have developed software for an STM32F103 target using Eclipse/OpenOCD/Olimex ARM-USB-OCD. Recently my hard drive failed so I replaced it and re-installed everything. My project will not now ru...

DMA into GPIO peripherial

Posted on June 10, 2014 at 16:54Hi all, I have a project where I need to deal with 4-to-8 bit and 8-to-4 bit conversion and so I have a questions: 1. I know that I can do DMA to/from GPIO but what is maximum speed of that operation. Can I go up to 2...

pawwodko by Associate II
  • 1758 Views
  • 3 replies
  • 0 kudos

Problem with STM32F103ZE SPI data send

Posted on June 04, 2014 at 04:47Hello I am trying to send opcode bytes MCBSTM32 to GP22. But as I debug in Keil I observe the the byte to be sent(0x50) is nit being written on the SPI data register in stm32f10x_spi.c. Instead the data register is sh...

CPU,DMA UART Transfer Independently

Posted on June 05, 2014 at 22:21Hello,       I want to transmit 10000 samples taken by adc continuously stored in an array. Is it possible the DMA-UART can transmit this to the PC while the CPU can take the next set of samples(independently) i.e wit...