STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS302DL MEMS: How to use INT1 and INT2 outputs

Posted on August 06, 2014 at 16:06Hello everybody !I try to use the LIS302 (the mems accelerometer of the discovery board).On the datasheet, I don't understand what are the outputs INT1 and INT2, what are the differences?Thanks for your time :) #...

jean by Senior
  • 4257 Views
  • 9 replies
  • 0 kudos

Encoder Interface with STM32F4

Posted on August 08, 2014 at 20:16I am trying to interface a quadrature encoder with my stm32f4. The code is almost the same as available on ''micromouse'' or many of the other forums. The major problem I am facing is: In debug mode I am able to se...

furqan by Associate II
  • 4515 Views
  • 9 replies
  • 0 kudos

STM32F071CB

Posted on August 07, 2014 at 12:20Hi, I already got a project working based on the STM32F030 and with Keil MDK. I based the project on a sample, so it was easy to get a working project. This time I don't have a discovery board with the STM32F071 and...

STM32F4 and LSM303 no reading data

Posted on August 10, 2014 at 14:48 Hi all, i recently started working on a orientation project using iNemo aplication, despite the dificulty of using pre build sensor libs, i said ''i`ll build my own''. Said and done, but when i try to r...

0690X00000604trQAA.png
Bogdan by Senior
  • 1211 Views
  • 1 replies
  • 0 kudos

SWD layout

Posted on June 12, 2014 at 00:53Does ST have any layout recommendations for using their Serial Wire Debug capability?  We are planning on using the Cortex M ETM debugging functionality.  This includes using the TRC CLK, TRC DATA[0], TRC DATA[1], TRC...

stm32f4 encoder interface mode

Posted on August 09, 2014 at 06:51Hi there! I'm using my stm32f4 timer 5 in encoder interface mode. In reference manual it is written for CCxNP/CCxP pins that they should not written 11 (i.e. polarity of trigger on both edges) in encoder interface m...

DDS DAC

Posted on August 08, 2014 at 07:49Hello,        I am generating a sine wave by DDS method, but I dont know why the signal is flattering at the bottom.       Does anyone have any idea why is this happening. Thanks #stm32 #dac

0690X00000604zPQAQ.png

ADC Resolution

Posted on August 08, 2014 at 17:29ADC resolution 12 bits(with 16 bit buffer) works but 8 bit(with 8bit buffer) results in the code going into an infinite loop in the DMA ISR. __IO uint8_t buffer[1000];/* ADC Config*/  ADC_StructInit(&ADC_InitStructu...

s7v7n92 by Associate II
  • 2301 Views
  • 5 replies
  • 0 kudos

SDADC Limitations Explained

Posted on August 08, 2014 at 15:07After reading through the promotional material, datasheet and reference manual for the STM32F3's SDADC and spending a few days trying to obtain a 16KHz sampling rate, I believe some clarification of the limitations ...

kevin2399 by Associate III
  • 2982 Views
  • 7 replies
  • 0 kudos

large SDRAM access causing hardfault in stm32f429

Posted on August 06, 2014 at 11:49Hello there!I've interfaced 128 MB(16 bit data bus) sdram through fmc interface in my stm32f429 device. Initialization and everything seems ok. Reading/writing to sdram is ok for small chunks. But writing 12 MB or l...