Skip to main content
rrlal
Associate
January 15, 2014
Question

STM32F3 CAN Init

  • January 15, 2014
  • 1 reply
  • 565 views
Posted on January 15, 2014 at 23:21

Hi,

I am trying to move some code from STM32F1 to F3 and having problems with CAN bus initialisation.

My custom board has the STM32F303CC Cpu with a 32MHz crystal. CAN initialisation times-out on waiting for CAN_MSR_INAK when leaving initialisation mode in CAN_Init() function of the standard peripheral library.

I have a discovery board which has the STM32F303VC CPU on it and the same code from above runs fine. Thinking it was perhaps a crystal problem, I tried just using the HSI instead - same result.

I have gone over the hardware a few times and I am lost for ideas - any help appreciated :).

R

    This topic has been closed for replies.

    1 reply

    rrlal
    rrlalAuthor
    Associate
    January 15, 2014
    Posted on January 16, 2014 at 00:46

    Solved: Pin differences between the two devices meant using GPIO_AF_9 instead of GPIO_AF_7 :D