STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 TRST

Posted on October 07, 2014 at 02:36I would like to use the Cortex M debug connector to debug and program an STM32F205.  The 10-pin connector does not have a JTAG TRST pin.  Will it still work with the STM32F205?  I plan to use an OCD debugger if tha...

STM32 Series - Calculations of Timer Variables.

Posted on October 05, 2014 at 04:02This is a subject that seems to have a lot of confusion (I do not fully understand). How to calculate the Variables: Period Prescaler Duration if only a few other variables are known. At higher frequencies, for e...

STM32Cube Tool Chains

Posted on October 06, 2014 at 22:18I downloaded, installed and used your STM32Cube software, Great Stuff, but when it came time to generate the code I was given a choice of :EWARM IAR MDK-ARM Keil TrueStudio Atollic Tool chains, where is the GNU too...

KevinA by Senior
  • 1113 Views
  • 1 replies
  • 0 kudos

STM32 sends weird characters to COM ???

Posted on October 06, 2014 at 17:36Hello, I send a char string to com port using sym32f4( with 3 pins only: GND VCC TX) and listen using ''hercules'' program finded on the net. I get weird characters, took a screanshot and uploaded as attachment. Ca...

aybala5 by Associate II
  • 8376 Views
  • 14 replies
  • 0 kudos

Mising startup file

Posted on September 23, 2014 at 01:44Hi All,I have done a search to no avail on this:Using Keil tools and Cube 4.3.1 (STM32F407), generating the project results in missing the startup file - but only at random.The folder ''Application/MDK-ARM'' does...

STM32CubeMx STM32F3 CCM-RAM

Posted on September 10, 2014 at 00:31Hi,  I would like to know if there are the option to create a IAR project in the STM32CubeMx that use CCM-RAM to run interrupt routines. If not. Are there plans to add it in the future?Ari.

Asantos by Senior
  • 672 Views
  • 1 replies
  • 0 kudos

Clearing TIM OCxREF signal

Posted on October 04, 2014 at 22:23Reference:RM0090STM32F407xx Reference ManualRev6Section 17.4.7TIMxCCMR1->OC1M--PWM Mode 1,2Quote:''2: In PWM mode 1 or 2, the OCREF level changes only when the result of the comparison changes or when the output co...

dibs by Associate II
  • 1537 Views
  • 1 replies
  • 0 kudos

stack pointer incorrect

Posted on March 25, 2013 at 10:39Hi, We are trying to migrate from IAR Kickstart kit with IAR-STM32F207ZG-SK board to our own board. On our PCB we have STM32F207ZC mounted. The small test code is successfully downloaded with J-Link. Downloaded C:\da...

optifier by Associate II
  • 4369 Views
  • 9 replies
  • 0 kudos

Problems with programming STM via ST-Link SWD

Posted on October 05, 2014 at 10:08Hello, I use your microcontroller STM32F407(lqfp100) at my work. We develop at the research institute a system of control engine. I developed a program at STM32F4 Discovery. But when I developed my scheme where use...

External Voltage Reference? To get a most accurate ADC result

Posted on October 06, 2014 at 09:53Dear all,We are trying to use the on-chip ADC of STM32F407. We have read two appnotes, which are AN4073 How to improve ADC accuracy when using STM32F2xx andSTM32F4xx microcontrollers and AN2834 How to get the best ...

cyqdtc by Associate II
  • 1193 Views
  • 1 replies
  • 0 kudos