STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN – Message Conflict Detection

Posted on May 13, 2015 at 23:25I am building a CAN Analyser using the STM32F429. At present I am only using one of the CAN channels and I have I found that if there is a collision during transmission when the NART bit is set then the MPU continues...

Initialzation for STM32F207 with CMSIS RTX

Posted on May 20, 2015 at 13:35HI,I want to make a baseline code for STM32F207 with CMSIS RTX. I gone through the example code * * main: initialize and start the system */int main (void) {  osKernelInitialize ();                    // initialize CMS...

STM32 debug Step-by-Step Problem !!

Posted on May 20, 2015 at 11:08Hello, I realize a project using stm3210e_eval,IDE: CooCoxDebugger: ST-Link V2When I'm debugging step-by-step, the cursor it's not linear !! and I don't understant Why ! for example: the cursor is at the line 170. when...

STM32F4 Cryptographic Acceleration

Posted on May 19, 2015 at 23:52I am implementing a platform that must implement Datagram Transport Layer Security (DTLS).I have the option of using the STM32F439x which includes Cryptographic Acceleration describbed in the datasheet as: ''Cryptograp...

ssmail by Associate II
  • 1663 Views
  • 1 replies
  • 0 kudos

STM32 TImer 2 Channel 3 ICU Config

Posted on May 12, 2015 at 21:42I'm trying to configure the STM32F4 MCU to use Timer 2 Channel 3 as an Input Capture Unit to measure frequency on an external signal. But so far, I'm not able to trigger the interrupt: static void TIM_Config(void) {  ...

krithik by Associate II
  • 2585 Views
  • 4 replies
  • 0 kudos

stm32lxx i2c slave, what am I doing wrong

Posted on May 19, 2015 at 22:05I have a stm32l00rb that I have set up as a slave. I have a SoC with embedded linux that I am using as the master. I am trying to use i2cdetect on the master (SoC) to detect the slave (stm32lxx), but I am getting no re...

DIY STM32F429 Evaluation Board

Posted on May 19, 2015 at 09:31hello, i would like to introduce my self-made Evaluation Board for a STM32F429IGT6 (176 Pin LQFP) pictures are attached it's a 4 Layer 100mm x 50mm Board with onboard : 256MBit SDRAM 512kBit I2C-EEprom 16MBit SPI-Flash...

mc-4u by Associate
  • 2897 Views
  • 3 replies
  • 0 kudos