STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

timer in HAL - prevent auto-disable

Posted on June 10, 2015 at 13:56What is the best way to prevent __HAL_TIM_DISABLE being called when all the CCxE are 0 ? __HAL_TIM_DISABLE(htim); is called in virtually every TIM...._Stop function It would be useful to keep the counter running parti...

pbayton9 by Associate III
  • 749 Views
  • 0 replies
  • 0 kudos

Bluetooth module echo problem

Posted on February 10, 2013 at 20:24 Hello, i am working on labview communication with bluetooth module driven by STM32F4, and some how i can't make it work. I can easy send data to labview, but not other way around, i have no idea where pro...

linas2 by Associate II
  • 3808 Views
  • 11 replies
  • 0 kudos

Stm32F4Discovery and AK4556 audio codec

Posted on January 28, 2015 at 14:08 I’m having a problem with my project. The project is just a simple sound “loop�? It is a stm32f4discovery connected to a audio codec. They communicate over I2S3 in Full Duplex mode and the stm...

0690X00000602tYQAQ.jpg 0690X00000602tcQAA.jpg
rasmus by Associate II
  • 2902 Views
  • 5 replies
  • 1 kudos

SPI - one-way communication Slave->Master

Posted on June 09, 2015 at 10:54Hello everybody, In my current project I need to establish an SPI connection between an STM32F407 microcontroller (slave) and an AD7763 A/D converter (master). Before the ADC actually starts sending any data, its two ...

Powf (power exponent) don't return float values

Posted on June 08, 2015 at 13:03 Hi everybody, I use the function powf (that is supposed to return a float), included in the library #include <math.h> This is the definition of the function in math.h : float powf _PARAMS(( f...

Easiest Interface to Use With a Windows PC.

Posted on November 13, 2012 at 14:37Hi, I am using the MCBSTM32E evaluation board to control some motors. I want to use my PC (Windows XP) to drive/record test data. Does anyone have an opinion on which interface is easiest to set up for communicati...

lisa2 by Associate II
  • 6232 Views
  • 20 replies
  • 0 kudos

STemWin GUI_CopyRect

Posted on June 10, 2015 at 09:09I have applied STemWin library on STM32F429 with LTDC peripheral  and external SDRAM with controller FMC on TFT display 800x480 pixels (24bit RGB mode). It seems that everything works. Functions as GUI_FillRect, GUI_D...

jiri by Associate II
  • 645 Views
  • 0 replies
  • 0 kudos

Did I just brick my board with a WFI?

Posted on June 08, 2015 at 18:53Hi folks,I find I am no longer able to download code to my target system (custom board) Using an IAR I-Jet on an SWD connector. The last code change I made was to add __WFI() to the end of my main loop.In this thread ...

hbarta2 by Associate III
  • 2013 Views
  • 5 replies
  • 0 kudos