STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 discovery and ST-link utility

Posted on June 12, 2015 at 08:27 Hello I'm trying to use the STM32F0 discovery with the ST link on board. So in first time, I try with ST link utilityV3.6.0 with STLinkUSBDriver.dll V4.3.4.0 on windows 7 pro 64 bits. All seem to be rig...

stm32f407 exti latency

Posted on June 24, 2015 at 17:54i am trying to communicate with ata device (via 40 pin ata interface) from my f407. with no prior knowledge to how the ata signals timing is, i used my logic sniffer to see the timing constraint. the strobes (for read...

STM32F4xx I2C ack bit voltage level problem

Posted on June 25, 2015 at 14:57HiI'm trying to get the STM32F427 I2C module (using I2C2) to communicate with a slave device and when I send a start bit followed by the slave address I can see that the slave device is trying to acknowledge on an osc...

STM32 c programming example

Posted on June 25, 2015 at 07:58dear all, i am bit confused in understanding the register handling of stm32 controller using c language. i am using keil compiler. i like to read, write register and set or clear single bit in the register. i want to ...

kumaresh by Associate II
  • 3101 Views
  • 3 replies
  • 0 kudos

STM32F427 CAN Remote Request

Posted on June 22, 2015 at 14:48I am not sure if I am in the right Forum for this problem but have seen a similar problem in another STMF4xx. I am configuring CAN bus and have a CAN message with Data as 'Remote Request, I have used Cube MX in uVisio...

Audio_playback_and_record

Posted on June 15, 2015 at 14:09 i want to build Audio_playback_and_record project for usb library but there are some problems. i downloaded this project (stsw-stm32zip) from http://www.st.com/web/en/catalog/tools/PF257904#. i have changed...

0690X00000603KcQAI.jpg 0690X00000603KhQAI.jpg

STM32F4 ADC Triple Mode with DMA

Posted on June 24, 2015 at 16:11The original post was too long to process during our migration. Please click on the attachment to read the original post.

pant by Associate II
  • 1392 Views
  • 2 replies
  • 0 kudos

Boot other than main

Posted on June 23, 2015 at 10:08hi ,i would like to  change the settings in coocox to run from a seperate file not from the main.can anyone tell me how to do that ?thanks 

arunl4g by Associate II
  • 1846 Views
  • 6 replies
  • 0 kudos