STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to configure ADC Dual mode to be as fast as possible

Posted on August 11, 2015 at 20:21Hi.Currently, I have configured ADC regular simultaneous dual mode for 8 AD conversions. 4 of them on ADC1 (master) and other 4 on ADC2 (slave). I transfer results via DMA as 4 32-bits words into my destination arra...

matic by Associate III
  • 1244 Views
  • 4 replies
  • 0 kudos

USB Data Transfer at High Speed

Posted on August 11, 2015 at 12:28Good afternoon to everyone!I want to develop a system around the stm32f4discovery hardware (I own this board) that acquires data from peripherals (one IMU, GPS and internal ADC) and ships it through USB to a HOST PC...

pedro2 by Associate II
  • 5181 Views
  • 7 replies
  • 1 kudos

Flash page erase problem. stm32f103vb

Posted on August 11, 2015 at 18:26Im having an issue erasing pages of flash. During my bootloader application while receiving a block of data I erase the page and then write the data. During testing I have the messaging protocol setup to just read t...

USART example code for Nucleo F401RE

Posted on March 26, 2014 at 04:16 Via Virtual COM port built into ST-LINK // STM32 USART2 (Tx PA.2, Rx PA.3) STM32F401RE NUCLEO - sourcer32@gmail.com #include ''stm32f4xx.h'' /**********************************************************...

SPI Status Flags Don't Update

Posted on August 09, 2015 at 20:09 I'm sitting here pulling my hair out because I can't figure out what's going on, I've tried everything I can think of. I'm using SPI to communicate with an offboard periph, When I write to the data register the...

Use of the same port both input and output

Posted on August 06, 2015 at 13:19 Hello, I need use a port both input and output. What should I do? Should I use something like this? GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_Ini...

fenice-6 by Associate II
  • 4723 Views
  • 8 replies
  • 0 kudos

PCROP protection

Posted on March 20, 2015 at 16:30 For our customer I need build a new hw with a ST micro (STM32F4) with a pre-porgrammed code library. The client develops its own application using the preloaded library (Obviously I provide also all the necessa...

Circular DMA data looks like rubbish

Posted on August 11, 2015 at 11:28 Hi, I'm using DMA with Timer2 input capture to sample the (ch2)rising and (ch1)falling edges of a 250kbps signal. So a bit is 4us long. When running the DMA in normal mode, the values make sense a...