STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401RB SDIO

Posted on August 05, 2015 at 20:37Hi all, there is something wrong with my project's microSD card part. I have done it on the  STM32F407 discovery board and it worked perfectly the data was succesfuly written to the microSD card. But for the end pro...

matas by Associate II
  • 4108 Views
  • 13 replies
  • 0 kudos

STM32F446 DMA Mem to GPIO

Posted on August 12, 2015 at 02:12 I have the example from the library showing DMA (mem to mem) working with the following initialization: /* Configure DMA Stream */ DMA_InitStructure.DMA_Channel = DMA_CHANNEL; DMA_InitStructure.DMA_...

daniel2 by Associate II
  • 5906 Views
  • 14 replies
  • 0 kudos

STM32-MP3NL/DEC Audio Engine MP3 Decoder and Utilities ?

Posted on August 12, 2015 at 23:49Hi Guys, I read about STM32-MP3NL/DECAudio Engine MP3 Decoder and Utilities in this link : http://www.st.com/web/en/catalog/tools/PF250969 Where can I find the software ? Is it not free ? Or I need an external chip ...

Basic questions about Alternate Functions

Posted on August 12, 2015 at 10:38Hi all,I am a beginner of MCU, and right now is digging into STM32F1xx serial MCU, which is pretty old, but simple enough for beginner. I have spent a lot of time on some example codes, still with the confusion that...

laojian by Associate II
  • 5372 Views
  • 5 replies
  • 0 kudos

Setting interrupt ADC conversion is complete using HAL

Posted on August 05, 2015 at 11:37STM32F407VG When Interrupt function looks like this:void ADC_IRQHandler(void){adc=HAL_ADC_GetValue(&hadc1); HAL_ADC_IRQHandler(&hadc1);  HAL_ADC_Start_IT(&hadc1);}Everything works well.But when I want to do the ADC ...

Fatal error: ST-Link, no MCU device found session aborted

Posted on August 10, 2015 at 11:26Hi When I configure the I2C to my code, my code is only using TSC, RTC, timer2 and sixteen GPIO. I compiler it that variable parameter is became ''unavailable'' in live watch windows. After that, I want to leave deb...

countach by Associate II
  • 4647 Views
  • 7 replies
  • 0 kudos

PWM with 1.5 MHz with STM32F411 Nucleo-Board

Posted on August 12, 2015 at 09:24Hello,i'm glad to be a member here in this forum. At the moment i am thinking about to buy a STM32F411 Nucleo-Board.  In this case i would like to ask you some question about this Board. I read many different articl...

mirco2 by Associate
  • 1838 Views
  • 2 replies
  • 0 kudos

HAL Vs Firmware

Posted on August 11, 2015 at 14:22Can anyone help me in understanding difference between HAL and firmware,I can find plenty of examples useful for starter as complete project in HAL related stuff, while no such thing available for firmware stuff (at...

waheed901 by Associate II
  • 3132 Views
  • 8 replies
  • 0 kudos

STM32L151 LSI clock accuracy

Posted on August 12, 2015 at 10:54HiRM0038 Reference manual sais: ''LSI clock ... The clock frequency is around37 kHz.''Can you tell me what is the max possible clock Deviation? (in percentage / Hz)ThanksYaron #stm32

yarona by Associate II
  • 2835 Views
  • 6 replies
  • 0 kudos