STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Interrupt/DMA/Array issue

Posted on September 03, 2015 at 19:21 I'm having a problem where when I try to access an array from within a timer interrupt callback, everything seems to fall apart. To keep it simple, I have: Timer 2 is set up to interrupt every 10us. ...

joesnyder by Associate III
  • 1860 Views
  • 3 replies
  • 0 kudos

STM32F410 new devices

Posted on September 03, 2015 at 09:32Hello,in new HAL drivers in Cube 1.8.0 for F4xx, I found some defines for STM32F410Tx, STM32F410Cx and STM32F410Rx. I didn't found anything on st site so I'm wondering if there will be new series and why is nothi...

tm3341 by Associate II
  • 1232 Views
  • 1 replies
  • 0 kudos

STM32F205 TIM1 Problem

Posted on August 22, 2015 at 13:26 Hello, I have a problem with my initalisiation code for an STM32F205RB Microcontroller. I want to use four PWM Output Channels on the TIM1, but only the Channel 4 work properly. The other channels d...

tih by Associate
  • 1697 Views
  • 3 replies
  • 0 kudos

Slave mode trigger on STM32F411RE

Posted on September 02, 2015 at 15:38Hi, I'm trying to enable the timer 2 on a rising edge of a signal that i have connect on the tim2_ch1. I understand that the slave trigger mode of the timer can do that. I want to generate a signal on the tim2_...

STM32F0 UART problem

Posted on September 03, 2015 at 11:22Hello,I'm using STM32F030 in my project. I'm using UART2 with Tx and Rx interrupts. While debugging, it works well but when i work it standalone, it stops before transmitting data and microcontroller probably sto...

omeryaman by Associate II
  • 1203 Views
  • 1 replies
  • 0 kudos

IAP for STM32F0 using STM32Cube

Posted on September 02, 2015 at 15:04Hi, I am wondering if there is an example for IAP using cube for STM32F0? I have found an example for STM32F1 and modified it for my board, STM32F070rb nucleo. I can load an application using the iap, but I have ...

seed by Associate III
  • 2280 Views
  • 4 replies
  • 0 kudos

How to Secure FW and keep IAP function

Posted on September 01, 2015 at 05:48Dear Sir:  My project use STM32F427. The project contains bootloader and main application. The bootloader can be used to update the main application.    Now I want to secure the application. I use Jlink secure ch...

Bootloader without pins manipulating / compilation issue

Posted on September 02, 2015 at 13:10 Hello, I am using STM32F401 Nucleo Board. I want go into the bootloader without pins manipulating. According to the many posts, I have seen in the forum. I added this code to my startup_stm32f401xe.s...

tingting by Associate II
  • 1118 Views
  • 2 replies
  • 0 kudos

ADC Dual - Scan - Continuous mode at the same time ??

Posted on September 03, 2015 at 09:18Hi. Does anyone know, if it's possible to use the mentioned combination? I have 8 Channels - 4 on ADC1 and 4 on ADC2. If I have Continuous mose disabled, it works nicely. I make two parallel AD sequences on both ...

matic by Associate III
  • 643 Views
  • 0 replies
  • 0 kudos

STM32L4 OTG_FS_VBUS issues again

Posted on September 01, 2015 at 22:23I am planning to use STM32L4 on a device powered by two alkaline batteries, and I'd like to use USB OTG. After reading the docs, i have came across a few problems:The first problem is the limitation regarding the...

dimitri by Associate II
  • 1499 Views
  • 1 replies
  • 0 kudos