cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F437 Vbat failure detection

petertroester9
Associate
Posted on March 16, 2015 at 17:21

We are using the internal RTC backed up by a goldcap.

In case of a power outage the backup voltage becomes lower by increasing time and at some time the oscillator stops running, but the RAM still remains valid for some time. So a magic number in RTC-RAM doesn't catch this. If the power returns while RTC-RAM is still valid everthing appears to look fine, but the RTC counter has stopped for an unknown time.

How can I detect the (potential) loss of time if RTC-voltage decreases?

Any idea is appreciated.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on March 18, 2015 at 09:50

The 'F4 is not very well suited for low power operation and for RTC, consider a battery rather than a supercap.

The voltage of VBAT can be measured by ADC, e.g. in a periodic wakeup. This of course would increase the current consumption - not only the core must wake up and start the ADC, but also the VBAT measurement involves connection of a divider to VBAT which sucks additional power from it.

Some other STM32 models also have a clock-security circuitry for LSE, in 'F4 there's no such (only on HSE).

You could also consider using IWDG refreshed from a periodic wakeup triggered by RTC, i.e. once RTC stops, IWDG bites. This also involves extra power.

You could also try to use an external micropower voltage detector.

JW
petertroester9
Associate
Posted on March 30, 2015 at 08:49

Thank you for your proposals.

In case of a power fail there is no way to wake up. So this approach unfortunately won't work.

A change in the hardware configuration is beyond of scope as well.

So maybe I must remain with my current approach to store the actual time in a nonvolatile memory every second as long as the system is powered. After the return of power I check if the RTC is within a window of time where I can make shure Vbat is still valid.

Unfortunately this binds me to the lower limit where I hoped for a way to reach the upper limit.