STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Infinite_Loop problem with STM32F030CCT6

Posted on September 18, 2015 at 00:31Hi all ST users.We have just replaced the STM32F030C8T6 microprocessor on some of our working boards to upgrade them with the larger STM32F030CCT6. A difference that should be both pin-compatible, periphiral comp...

0690X000006034ZQAQ.jpg

STM32F746IGT: Booting from FLASH Sector 4

Posted on September 10, 2015 at 23:46Hello all,I am looking how I can flash my firmware to sector 4 (0x0802 0000) and jump to it to execute the code.  I am using Keil uVision 5 as development environment.I know that I must changed the address in the...

keaven by Associate II
  • 774 Views
  • 2 replies
  • 0 kudos

Power management circuit for STM32F103

Posted on June 01, 2012 at 10:59Dear all,I need to design a board based on STM32F103RE.My board need to be powered in two ways, USB & Li-Ion 3.7V battery. In addition i need to design a IN-BUILT battery charging circuit( USB to Li-Ion battery) for t...

harinath by Associate III
  • 2883 Views
  • 2 replies
  • 0 kudos

creat project virtual com port

Posted on September 16, 2015 at 11:01Hello, please give me the procedure to creat a project virtual com port(usb cdc) with STM32CubeMX. (STM32F429discovery)I followed the steps but according to manager level péréphirique the material is unknown:Proc...

med by Associate II
  • 2222 Views
  • 4 replies
  • 0 kudos

HAL gpio libary code bug

Posted on September 04, 2015 at 09:24This problem has been reported in the following link.https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%...

dan2 by Associate II
  • 3186 Views
  • 7 replies
  • 0 kudos

STM32L152 Nucleo Reading 16-bit Sensor Register

Posted on September 17, 2015 at 13:36I am using STM32L152 Nucleo (Nucleo L152RE) with ALS sensor connected to it.ALS sensor has a 16 bit data register containing both MSB and LSB .Below is the register Map        0x04 15:8 MSB Data of whole ALS 16bi...

darla14 by Senior
  • 591 Views
  • 0 replies
  • 0 kudos

rtc bug stm32 cube l0

Posted on September 17, 2015 at 07:41Hello, I have implemented RTC on STM32l053-Nucleo using CubeMX and CubeL0 HAL libraries. I set and get the time and date in RTC using HAL functions but the RTC is not running, I am getting the same time and date ...

STM32F429ZIT6 flash problem

Posted on September 17, 2015 at 11:13Hi. i got issue with flashing my MCU. I add my scheme. It is soldered on prototype board, not in real PCB. I cant download program to MCU ''Error: Connect failed, check config and cable connection''. All componen...