STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L151 and microSD card

Posted on September 24, 2015 at 01:10Hi,I want to connect a microSD card to my STM32L151CBU6 MCU and read/write data to this uSD card. I have made the schematics, but I am unsure if I have connected the uSD card holder correctly to the MCU (see atta...

0690X000006031MQAQ.jpg
lrsolem by Associate
  • 1075 Views
  • 0 replies
  • 0 kudos

Forum acting quirky today

Posted on September 17, 2015 at 19:00Not sure if ST changed some settings, but I'm getting a lot of errors when posting, or when I open an new tab against a link (ie navigating back to a post from hyperlinks provided on the page, or edit window, to ...

cubexmx usb hid code generation for stm32f411

Posted on September 02, 2015 at 23:10 Hi I have a custom board with a stm32f4 I am trying to use cubmx to generate a usb HID project but the generated code does not work. The board appears as an unrecognized device when I attach it to my com...

0690X00000604WWQAY.png 0690X00000604s6QAA.png
ruairi by Associate
  • 2768 Views
  • 5 replies
  • 0 kudos

STM32F4xx RTC questions

Posted on September 21, 2015 at 16:49All:First, I have been able to ''setdatetime'' and ''getdatetime'' using excellent example code. In fact, I wait until after powered up to receive a ''setdatetime'' command (via UART). Using the HSE on F4 Discove...

tba10596 by Associate II
  • 2051 Views
  • 3 replies
  • 0 kudos

STM32L476QE Flash write and Erase API

Posted on September 10, 2015 at 14:12We are using STM32LL476QE and as per reference manual , While executing a program code from bank 1, it is possible to perform a program operation on the bank 2. Here we are into situation in which Our custom Boot...

CAN message transmission problem

Posted on September 18, 2015 at 08:43Hello all, I wrote code for CAN message transmission using STM32F429ZI board. Message is not getting transferred. It is displaying only error frames in CANanalyzer. Please suggest me solution for this problem. I ...