Skip to main content
bharadwajtke
Associate II
April 27, 2015
Question

With STM32F429I-DISCO Along side of ''IS42S16400J SDRAM'' Connecting another FMC Device?

  • April 27, 2015
  • 2 replies
  • 667 views
Posted on April 27, 2015 at 16:19

Dear All,

Is it Possible to Connect another FMC device along side of IS42S16400J in STM32F429I-DISCO

board, does the Address line and Data line causes any problem to the other FMC device from the onboard SD RAM(IS42S16400J )

Note: External device Voltage is same as the SDRAM Voltage level, Control lines are different for the External interfacing device,Except Data and the Address bus are shared Between SDRAM and the External FMC device.

Thanks for your valuable response, in advance.

#stm32f429i-disco-fmc-is42s16400j
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
April 27, 2015
Posted on April 27, 2015 at 16:27

Yeah, you'd want to be attentive to signal lengths and termination. Access to the pins on the DISCO might be a tad challenging.

Suggest you review the schematics for the

http://www.st.com/web/en/catalog/tools/PF259093

which uses several memories.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
bharadwajtke
Associate II
April 28, 2015
Posted on April 28, 2015 at 07:13

Hi CLive,

Thank you very much for your suggestion, you have been very active in this blog always you have been giving right suggestion and Input.

Thanks for your help.

Please tell me how can show my gratitude of your help, so it will help you and others.

I am very happy for your help to all these forum recipients.

Thanks again :)