STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32: how to use an nrf24l01 transceiver

Posted on March 26, 2015 at 07:20Hi to all, I have two stm32f3 discovery with 1 nrf24L01 transceiver on each one.  I want to send a packet from one and receive this packet on the other one. Can someone help me? I have no idea. Thanks...

vito by Associate II
  • 8667 Views
  • 12 replies
  • 0 kudos

STM32F7 Discovery Blinky Project fails and BSP errors.

Posted on October 12, 2015 at 16:03I wanted to make a blinky example (LD1) on my STM32F7 DIscovery using HAL drivers as HAL_GPIO_WritePin(GPIOI, GPIO_PIN_1,GPIO_PIN_SET); with no result, then i resolve that i could use BSP drivers, but i had this er...

Test/Clear EV7 i2c Std Peripheral Library- Help!!!!

Posted on October 12, 2015 at 17:59Hi,I think I have traced my problem with my big combined i2c DMA project.I need to test on EV7 and clear it after receiving every byte - but the Std Peripheral Library firmware doesn't seem to have a command for th...

estersci2 by Associate III
  • 1328 Views
  • 2 replies
  • 0 kudos

C# netFM: system.security leads to crash...

Posted on October 12, 2015 at 11:33Hi, I want to implement some encryption functions on the STM32F429Discoveryboard using the netFM ''system.security'' or ''microsoft.SPOT.security.PKCS11'' assemblies (VS2012). The problem is: if I add the assemblie...

CubeMX, template for other Ethernet Phy

Posted on May 03, 2015 at 20:16Hi, I have an Olimex E407 Board with STM32F407ZG and PHY LAN8710A. If I make a Project in CubeMX the stm32f4xx_hal_conf.h is generated for DP83848 PHY from stm32f4xx_hal_conf_template.h in Repository\STM32Cube_FW_F4_V1...

Peter15 by Associate II
  • 1598 Views
  • 2 replies
  • 0 kudos

STMF7 (100 LQPF) Missing LCD pins

Posted on October 09, 2015 at 11:18Hi, Im currently evaluating which STM32F7 controller for use in a HMI project. I was studying the connections required for the 24bit LCD interface on the STM32F746VG (100 LQFP). Looking at the GPIO alternate fun...