Question
UART receive interrupt
Posted on April 22, 2015 at 19:02
I have a board using an STM32F105. There is a GPS connected to UART4. I've been trying to get the RXNE interrupt working for a couple of days now, but I must be missing something.
The UART seems to be enabled, as I can send data. It doesn't get to the receive interrupt, though. I wrote some simple code to poll the UART and to take any data received and then transmit that data. No matter what data is present on the bus, the data sent is 0x00. Because of this, I think that I have something set incorrectly in my UART configuration. Can someone please have a look at the setup and give me a nudge in the right direction? Thanks! USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); //RCC_APB1PeriphResetCmd(RCC_APB1Periph_UART4, ENABLE); /* Configure USART pins */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; //TX GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; //RX GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOC, &GPIO_InitStructure); /* UART configuration */ USART_DeInit(UART4); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(UART4, &USART_InitStructure); //select NVIC channel to configure NVIC_InitStructure.NVIC_IRQChannel = UART4_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 13; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_SetPriority(UART4_IRQn, NVIC_EncodePriority(4,1,0)); NVIC_EnableIRQ(UART4_IRQn); USART_ITConfig(UART4, USART_IT_ERR, ENABLE); USART_ITConfig(UART4, USART_IT_RXNE, ENABLE); USART_Cmd(UART4, ENABLE); #stm32 #usart #receive