STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051 SPI problem, help

Posted on November 06, 2015 at 16:10Hi there,I'm trying to communicate to my SPI TFT LCD module. Previously I used to do it with an F4 discovery board, now I want to use an STM32F051 , here is my code:#include <stm32f0xx.h>#include <stm32f0xx_rcc.h>...

monta by Associate II
  • 779 Views
  • 0 replies
  • 0 kudos

STM32F07x, STM32F08x and STM32F09x are dummy products???

Posted on November 06, 2015 at 13:19Hi, I have a new project which would run on STM32F051K8T but need more than 64K flash. I saw the STM32F0[789]x has more flash but nobody sell them!? Mouser, Digikey,.... have not one of this series. Do somebody se...

Osto by Senior
  • 1293 Views
  • 2 replies
  • 0 kudos

STM32F334 SPI PROBLEM

Posted on October 31, 2015 at 08:48 Hello ; I am using spi with external ADC ; when I use bitbang spi I can communicate with the ADC and it is ok ; But I need to use harware SPI ; when I am using the internal SPI1 I cant communicate with t...

Please give me advice about how to use NVIC

Posted on November 06, 2015 at 12:55Hello. My colleague is in trouble about NVIC of STM32L053.. At the moment, he wants to use several external interrupts; some of them are assigned to EXTI line 0, some others are assigned to EXTI line 1, and the r...

There is problem with DCM colors

Posted on October 29, 2015 at 12:50 Hello, I have some problems with camera. At reception high and low bytes change places. It's make bad image (picture 1) First I think that I lose a first byte and by myself shifted a buffer on 1 byte. ...

0690X000006034oQAA.jpg 0690X000006034yQAA.jpg 0690X000006036kQAA.jpg

STM324x9I-EVAL for application with LCD as user interface

Posted on October 29, 2015 at 14:03Hi all.im about to work on a project which include an LCD as user interface and suppose to display images.LCD size is 240x320 pixels.im trying to use STeMWin tools - GUIBuilder and BMPCVT and FNTCVT.its seems like ...

asafbit by Associate II
  • 854 Views
  • 1 replies
  • 0 kudos

Flash - erases but won't write in application

Posted on November 05, 2015 at 19:43Im using the STM32F302vb with gnu tools and a jlink for programming and debugging.I'm am currently having an issue with a bootloader application which is a port from an F103 device that works. The problem I'm runn...

STM32f100: how start TIM1 interrupt handler

Posted on June 23, 2011 at 18:03Hi! I've to program STM32f100R4H6; particularly i've to manage TIM1 interrupt. Below there is my code..Thank you in advance.. ------------------------------------------------------------------------------------------...

How to conveniently read GPIO while it is in AF mode ?

Posted on November 05, 2015 at 17:59I'm interfacing with TI CC1101, it need to check MISO pin to low before start SPI transaction.Shall I change MISO pin to AF mode to Input mode before I read, and then change it back to AF mode to start SPI.Is  the...

sprhawk by Associate II
  • 2083 Views
  • 4 replies
  • 1 kudos

st link v2 error no elf loader found

Posted on October 27, 2015 at 22:06I just received my stm32f746g discovery board, tried to load a demo file and error pops up ''no elf loader found for this operation''. I have upgraded st link, and firmware but still get this error. How do I correc...

jara8462 by Associate II
  • 1885 Views
  • 2 replies
  • 0 kudos