STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Discovery TIM1 PWM Generation problem

Posted on July 22, 2014 at 22:03Hi, I've been trying to generate complementary PWM output on TIM1 Channel 1, but there is no example of this for the STM32F4 Discovery, so I wrote the code based on several examples for other chips/boards, but the cod...

yifan115 by Associate II
  • 3781 Views
  • 7 replies
  • 0 kudos

STM32F4 problem with CAN bus

Posted on November 19, 2015 at 15:54 Hi, I use an STM32F407 , I'm trying communication with CAN bus, for now only transmission , using Hal library. 1) I have setted PA11 (CAN1_RX) and PA12 (CAN1_TX): void...

vlr by Associate II
  • 1210 Views
  • 1 replies
  • 0 kudos

STM32L152-EVAL Board SD Card Files

Posted on November 18, 2015 at 16:19I got a STM32L152-EVAL board. Unfortunately the SD card is missing, therefore no demo software is running on the board. Has anybody a link or even the files that have been originally placed on the SD card? Thanks ...

mmetzger by Associate II
  • 1264 Views
  • 2 replies
  • 0 kudos

Vdd of STM32L100C-DISCO

Posted on November 17, 2015 at 15:31I have this board a couple of days. I am trying to blink LEDs. With green one it works fine, but with blue one it doesn't work.I think the problem lies in the 2V VDD. LED works if it is supplied by external source...

kozlovdmn by Associate II
  • 1060 Views
  • 2 replies
  • 0 kudos

STM32 Host USB Memory FatFs reads corrupt data

Posted on November 19, 2015 at 08:08I am on a project with an STM32F407 on a custom board and I am having trouble with reading from a USB memory device.The code framework is generated with CubeMX and setup to use FatFs and USB in host mode to access...

STM32F446RE can no connect to target

Posted on November 17, 2015 at 14:59Hello, this is my first post.It is the first time I use an STM32 Device, I am familiar with 32Bit processors of TI so far.I did a new PCB connected with the ST-Link programmer of a Nucleo board. But I can not conn...

hcls by Associate II
  • 2548 Views
  • 8 replies
  • 0 kudos

SPI to LCD FT800 not working well

Posted on October 26, 2015 at 04:42First i use Mode for SCK and MOSI was AF_PP but we read a strange value 0x42. and i Change it to AF_OD and it shows another value, that was 0xFE. and still not find the ready value of FT800 display. that should sho...

rifqi by Associate
  • 1037 Views
  • 2 replies
  • 0 kudos

STM32Cube two ADC with DMA problem

Posted on November 18, 2015 at 13:33Good morning everyone!I've been using STM32Cube code generator for a while now. Yesterday I've encountered a problem, while configuring ADC converters using DMA.When I configure one converter with DMA and few chan...

0690X00000604szQAA.png
bartek by Associate
  • 978 Views
  • 1 replies
  • 0 kudos

Inaccurate timer synchronization problem

Posted on November 18, 2015 at 06:54Hi everybody,I need to synchronise Timer1 and timer4 to each other, in my STM32F103.These slave timers are Triggered by Timer2 as Master timer. I even set the MSM bit of TIM2_SMCR to have better synchronization.I ...