STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f401re nucleo: PLL configuration

Posted on November 26, 2015 at 13:54Hello everybody!I'm trying to configure the main PLL to generate the max clock frequency (84 MHz on this board), and I'm using the HSI as PLL source.I made some test:- test1: HCLK=70 MHzM=16N=140P=2AHB_PR=1APB1_PR...

life758 by Associate II
  • 2200 Views
  • 5 replies
  • 0 kudos

HardFault while implementing USB MSC device

Posted on January 24, 2015 at 11:33Hi,I used the CubeMX framework to implement a USB mass storage device for my STM32L1 device.I see that the code is issuing a hard fault when the laptop connected to the device is reading sectors from the device dur...

bnp979 by Associate III
  • 1604 Views
  • 2 replies
  • 0 kudos

STM32 Ethernet DMA - chain and ring descriptor structures

Posted on November 07, 2015 at 22:24Hello.I am trying to understand a few things connected with the Ethernet peripheral (more precisely � its dedicated DMA) which can be found in some STM32F4 devices. In this post I am referring to the http://www.st...

szczepan by Associate
  • 2922 Views
  • 1 replies
  • 0 kudos

LPTIMx_CMP interrupt on STM32L476

Posted on November 17, 2015 at 20:07I'm trying to generate an interrupt on compare match of LowPower Timer. No luck until now, I tried everything using the HAL libraries, the AutoReload interrupt is correctly generated but not the compare match. Any...

angeletti by Associate II
  • 1354 Views
  • 1 replies
  • 0 kudos

Prinft and STM32F103z and STM32Cube?

Posted on November 17, 2015 at 15:28 I start with STM32F and create my first ''Hello Word'' application a have problem with printf. My dev.board is http://www.waveshare.com/wiki/Open103Z IDE Keil MDK-ARM 5.17 In the STM32Cube I cr...

UART example code for STM32F0

Posted on November 20, 2012 at 23:34Hello, I looking for some example code for communication between my ST-DISCOVERY F0 board and PC (UART). Can someone help me with it? I´m novice.Thank you

hospodar by Associate III
  • 21131 Views
  • 60 replies
  • 0 kudos

STM32F401 wake up with Periodic mode

Posted on November 07, 2015 at 17:25 Dear gentelmen, I'm quite new in this ''PowerSaving'' area and looking for your support. I work on application where stm32f401 have to wake up every predefined period of time(30min-24h), do some job an...

sshults9 by Associate
  • 1183 Views
  • 1 replies
  • 0 kudos

NVIC_SystemReset stuck

Posted on November 24, 2015 at 14:09Hello,I'm currently working on a STM32F302VB and I need to perform a Soft Reset. On previous projects with STM32F030C8 and STM32F407, I've used the NVIC_SystemReset() function without any problems, but for some re...

florent23 by Associate II
  • 2635 Views
  • 2 replies
  • 0 kudos

STM32F429 HAL_UART_Receive_DMA problems

Posted on November 25, 2015 at 19:08Hello,I have an issue to which I cant find a solution.I'm working with different UARTs, and I find a problem. If I use them using HAL_UART_Receive_IT, everything works ok, HAL_UART_RxCpltCallback is called, etc et...

fb2 by Associate II
  • 1350 Views
  • 2 replies
  • 0 kudos