cancel
Showing results for 
Search instead for 
Did you mean: 

SPL for F0xx, V1.5.0 .chm help file has missing info (19/Jul/2015)

uc2013135191
Associate II
Posted on July 19, 2015 at 02:10

Just wanted to give a heads up to this.

First of all, I am sorry if it was already referenced but I could not find anything when using the search tool.

I have the V1.5.0 standard peripheral library package for F0 series. I also have V1.4.0.

One thing I noticed is that the V1.5.0 is missing all the drivers info!

There's nothing there as far as I am aware, when I got to ''Modules'' there is nothing there for them, when I searched for it further I had no success in finding the information. 

I downloaded again the package and as of now, July the 19th of 2015, the problem still persists.

To note that in V1.4.0 there was also a problem with it, the info for the timer drivers was not present in the correct place, and was instead on the page before it, named ''STM32F0xx_StdPeriph_Driver''.

I find that help file really useful and wanted to bring attention to this problem with hope it is fixed. I know most of that info can be found in the source files btw.

#.chm-f0-spl-library-help-file
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on July 22, 2015 at 12:16

Hi,

You are right;all the drivers info is missing.

It is noted and will be fixed in coming release of the STM32F0 standard peripheral library.

-Syrine