STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

reverse supply through output

Posted on December 08, 2015 at 23:19My STM32F030 is SPI slave to another external MCU.  External host may turn the VCC of my STM32  off.  When this happens SPI_CLK and MOSI pins are still at +3.3V, and these signals back-supply my MCU through output...

STM32F4 RS485 and RTS pin

Posted on December 08, 2015 at 12:11Hello there,I need to implement rs485 communication using STM32F407. I am using MAX487 chip which has a direction pin. I have searched the forums for a hardware solution to this, and found a topic which says that ...

0690X00000605K1QAI.png

CubeMX broke SDIO DMA in latest update

Posted on November 12, 2015 at 15:04In the current release of CubeMX V4.11.0 using the latest F4 libraries, V1.9.0, a bug has been introduced that makes the SDIO DMA channels useless.  In the previous library set, V1.8.0, when the DMA channels were ...

STM32 NUCLEO extension board with Ardunio Uno

Posted on November 10, 2015 at 21:05Hi ,I am trying to develope Ble HID keyboard using Ardunio Uno and STM32 X-NUCLEO-IDB05A1 extension board.I am very new to this... I have gone through the STM32 quick guide. I could not understand whether I need t...

venky999 by Associate II
  • 1223 Views
  • 3 replies
  • 0 kudos

SPI

Posted on December 08, 2015 at 16:01

arunease by Associate II
  • 944 Views
  • 1 replies
  • 0 kudos

STM32F249 ADC using EXTI11 + DMA

Posted on December 08, 2015 at 12:08 Hello, I'm trying to use ADC with EXTI_ I have read many discussions before but still got an issue here. Here's the code I'm using: static void ADC3_CH13_DMA_Config(void) { ADC_InitTypeDef ADC_I...

Sector and page size on STM32F072C8

Posted on December 08, 2015 at 11:30I need to find out the sector and page size on my particular SOC, which is STM32F072C8T6. According to the part number information from the data sheet (DM00090510), this is a 64 kB flash memory version. From the r...

gmate1 by Associate II
  • 2845 Views
  • 3 replies
  • 0 kudos

DWT_CYCCNT -- explanation

Posted on December 08, 2015 at 13:08 Hi i have seen the below code on this forum. for example if i wnt to make a delay for 10 seconds then how to calculate the tick value.? Can anyone help ?. volatile unsigned int *DWT_CYCCN...

arunease by Associate II
  • 1073 Views
  • 3 replies
  • 0 kudos