STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART does not get interruption from time to time.

Posted on December 14, 2015 at 10:41Hi, We are using an ARM STM32L100RC. We receive in our firmware a message of just two characters through the USART 1. At 9600 kbps it works ok, at 19200 it fails sometimes, but at 38400 it fails one in ten times (...

rvarona by Associate II
  • 2030 Views
  • 4 replies
  • 0 kudos

Same calculation time in both 36MHz and 64MHz

Posted on December 15, 2015 at 14:55Hi everybodyI am trying to implement some mathmatic calculations in STM32F103.I use HSI and PLL to provide 64MHz and 36MHz clock, considering Flash Wait State and enabling Prefetch Buffer. I expect that the calcul...

serial port debug question

Posted on December 12, 2015 at 16:29Hello All, Moving from the Motorolla 9s12 to the stm32.  Just got a eval board and after recovering from Register shock I am just trying to get some blinky lights and serial comm (USART) going which is what I wou...

USB Host HID EventCallback

Posted on December 15, 2015 at 12:16Dear,In my STM32F429 application I use a mouse or a keyboard The USBH_HID_EventCallback is common to both It would fine to have a different callback registered in the HID_Handle by USBH_HID_InterfaceInit() like it...

EXTI rising falling with pin monitoring - issue

Posted on December 15, 2015 at 10:05 I'm using STM32F4 Discovery. I configured a GPIO pin PB8 for external interupt for both rising and falling edges, so that I have to reset a flag when it is high->low or set when low->high which is done by rea...

Problem Failed firmware STM32F7Disco

Posted on December 15, 2015 at 10:34Hi. Board http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/LN1848/PF261641?icmp=pf261641_pron_pr-massmarket_jun2015&sc=stm32f7discovery-pr On board I found this file: FAIL.TXT - ''The interface firmware F...

how to set RTE in uVision5

Posted on December 15, 2015 at 03:46Hi, in the uart_printf example project(using HAL drivers), I see the RTE(Run Time Environment) for the project has all the entries below not selected(empty) which seems weird to me. What do these empty entries mea...

0690X00000602akQAA.jpg
ckim by Associate II
  • 1128 Views
  • 0 replies
  • 0 kudos

F407VG And Its UOTGFS

Posted on December 13, 2015 at 01:59 Workalot is struggling with enumeration of an USB VCP application. While USBRST and ENUMDNE interrupts are being captured no other interupts are. Perhaps a kind observer may glance over the register settings ...

Workalot by Associate III
  • 1105 Views
  • 1 replies
  • 0 kudos