STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32-MP3NL-COD

Posted on February 09, 2016 at 17:04Hi, does anybody know where to get the STM32 Audio Engine ? http://www.st.com/web/en/catalog/tools/PF250970 Is it possible to get this for a student project ? Or are there any other demo projects availaible to pla...

timing if statement stm32

Posted on February 09, 2016 at 10:37I'm working on a porject where I need to communicate with an USB PHY chip. I am using a STM32 microcontoller. (stm32f446ret6,http://www.st.com/web/en/resource/technical/document/datasheet/DM00141306.pdf)To communi...

stijn2 by Associate
  • 2281 Views
  • 2 replies
  • 0 kudos

FFT problem on stm32f4 discovery.

Posted on August 29, 2015 at 19:08Hi. I am facing strange problem implementing FFT on stm32f4 kit. i am using Virtual Com Port to transmit serial data which is plotted on QT (C++) platform.The problem i am facing is that some time output is correct ...

ameer by Associate II
  • 2195 Views
  • 6 replies
  • 0 kudos

NVIC priority group, preemption and sub priority.

Posted on December 18, 2011 at 17:11What is the meaning of Preemppriority and subpriority? If the number allocated to them is higher, does it mean that they are prioritized for the service than the others which are allocated less number or it is th...

SWD problem ''Failed to read memory''

Posted on February 08, 2016 at 13:43 Hi! I am having problems when using SWD cables to read/write on my STM32F105RC MCU. The MCU is on a custom board. I connect with ST Link Utility but get the error ''Failed to read memory'' 0x080000xx. At ...

daha0902 by Associate II
  • 3145 Views
  • 2 replies
  • 0 kudos

Cannot build on STM32F429I_DISC)

Posted on February 08, 2016 at 04:42I am attempting to build for the first time with my STM32F429I-DISCO using eclipse and the STM32 standard periph. I set up my toolchain from the instrcutions http://thehackerworkshop.com/?p=1056. One thing I am st...

ejanuska by Associate II
  • 2057 Views
  • 3 replies
  • 0 kudos

RTC subsecond interrupt does not work

Posted on February 08, 2016 at 19:33I have written some code to generate an interrupt from the RTC alarm. This includes sub seconds. This works well for times in excess of 1 second. The alarm time, including subseconds is calculated and displayed. W...

squin by Associate II
  • 1361 Views
  • 2 replies
  • 0 kudos

Parametric search - HSE available or not

Posted on February 07, 2016 at 21:33Hi, I have tried in STM32Cube and I have tried the online parametric search. I want to filter the STM32L0xxx parts so I only get those which have external HSE clock connections available. This ought to be possible...

soren by Associate II
  • 736 Views
  • 2 replies
  • 0 kudos

Java exception when running cube 4.8.0 on Linux

Posted on June 15, 2015 at 17:10 Hi, My STM32CubeMX.log file shows the following backtrace when I try to configure a GPIO pin and the panel at the bottom of the dialog that should show the configuration controls is empty. Exce...

markb by Associate II
  • 2887 Views
  • 8 replies
  • 0 kudos