STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Peripheral issues with STM32F103C8

Posted on February 11, 2016 at 13:24Hi,Sorry if I've opened a discussion on an issue already solved...I've recently started a new project on a board with STM32F103C8 on it (the small cheap 40 pin board from ebay). I made the base project with CubeMX...

paul90g by Associate
  • 740 Views
  • 0 replies
  • 0 kudos

STM32F4 /F7 USB HS PHY max speed

Posted on February 10, 2016 at 11:29Hi, at the moment im using a STM32F3 as custom FS HID device to send 1000 64byte packets each second (64kb/s) to host pc. i would like to increase the speed so im wondering which speed i can get with the external...

Memcpy vs DMA

Posted on February 10, 2016 at 16:47hi, I'm using the STM32f407-discovery board example of DMA_FLASH_RAM.I've noticed by using systics for time measurements, that memcpy provides better timing than DMA.for example.I have 16bit array of 64 elements t...

haukeye by Associate II
  • 7813 Views
  • 5 replies
  • 0 kudos

STM32F103x and MPU6050 I2C Issue

Posted on February 09, 2016 at 14:27I worked out on a library for UART debug and I2C basics to read write registers via I2C..problem now is I read the  FIFO but it turns out to be zero..Disabled sleep bit..Fifo Enable Register Set, User Control Regi...

strtod exception on STM32F746NG-Discovery

Posted on February 11, 2016 at 05:19I am using STMCube with an STM32F746NG-Discovery kit and the IAR tools.  I can build the samples with STMCube and run then but if I use strtod() then the application will crash in:_Stoflt + 0x113__iar_Stodx + 0x39...

brian2 by Associate II
  • 760 Views
  • 0 replies
  • 0 kudos

PWM output without using Timer as AF.

Posted on February 10, 2016 at 15:02I want to generate a PWM output for a GPIO pin without using Timer as the AF. Is there any other way of accurately doing this? Timers in other modes can be used. Code samples will be helpful. #output #pwm #disc...

STM32F373 SDADC Calibration hardfault

Posted on October 03, 2014 at 09:45Hello, I would like to kindly ask for a help with calibration of SDADC peripheral on chip STM32F373. Im using SDADC with TIM19 triggered conversions 1000Hz.  I have tried two variants of calibration A)     /* Set C...

ssubrt9 by Associate
  • 1153 Views
  • 1 replies
  • 0 kudos