STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

output compare with 32 bit timer

Posted on March 14, 2016 at 11:19Hello there, I have a question regarding output compare mode with 32 bit timers in STM32F4 mcu. I have only one 32 bit timer that is free to use. I need to generate interrupts for 2 events. Those events should occur...

STM32F SPI DMA transfer, triggered by Timer

Posted on March 14, 2016 at 10:54Hi everyone, I have some cpu-load issue on my design, so I am trying to redesign an high frequency Rx spi transfer. (24bit) I would like to setup a timer that at a certain frequency triggers the Rx SPI transfer. Righ...

stm32f407 and 3g/gprs module ?

Posted on March 14, 2016 at 11:12Dear All,I am using an stm32F4discovery ( stm324f07vgt)  to capture images coming from a camera OV5642, i would like to send pictures ( 5MP) with 3G module, Could you please suggest me an exemple of module that suppo...

STM32F37x DMA SDADC + DAC same DMA Channel

Posted on March 11, 2016 at 17:03Dear Community, I am trying to use two peripherals (STM23F373) SDADC1 and DAC1_1 having the same DMA access channel: DMA2_Channel3 (STM32F37x reference page 164). Due to a synch problem I want to use the DMA in norma...

jogerh by Associate II
  • 1213 Views
  • 2 replies
  • 0 kudos

Problem reading SD card

Posted on March 11, 2016 at 20:08Hi to all, I have a big issue with SD cards. I initialize correctly my sd card, but when I try to read a block, I can read it only the first time. This is my routine: ===================== uint32_t MYSD::ReadSector(u...

STM32F4 synchronise timer + generate variable frequency

Posted on March 07, 2016 at 12:56Hi, I have a litte problem. I need to generate a variable frequency (not duty cycle) for a piezo buzzer. Unfortunately the PCB layout is givn as a H-bridge (see image). ''Piezo'' is connected to TIM4_CH1 and ''Piezo2...

0690X00000605b6QAA.png
kruszi by Associate II
  • 1200 Views
  • 2 replies
  • 0 kudos

F1 can hal_can_state always 0x22

Posted on March 11, 2016 at 21:36  The original post was too long to process during our migration. Please click on the attachment to read the original post.

bartocham by Associate II
  • 1430 Views
  • 2 replies
  • 0 kudos

Anomalous high ADC rate at stm32f103cb

Posted on March 11, 2016 at 21:02 Hello! I need an advice. My stm32f103cb chip has ADC with 0.39 us per point conversion rate on one channel. But datasheet says its max rate is 1 Msps (1us). I checked sampling rate with external oscillograph (1 ...

STM32F051C8 UART2 or 1 don't trigged

Posted on March 13, 2016 at 01:59 Hello i'm trying to configure an uart 1 or 2 interrupt in sw4STM32 and cube mx, but never responses the interrupt i can recive data from uart and send data in uart 1 and 2 in pooling mode mi code. Main ...

enagma by Associate
  • 563 Views
  • 0 replies
  • 0 kudos