STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

i2c on fast mode hangs on stm32f103cb

Posted on March 15, 2016 at 02:35When reading data from an MPU6050 on standard mode (100khz) everything goes well, but when switching to fast mode 400khz the program just hangs, debugger shows an infinite loop on line 3935 of stm32f1xx_hal_i2c.c    ...

0690X00000605N9QAI.png 0690X00000605KGQAY.png 0690X00000605MqQAI.png
gvuyk07 by Associate II
  • 796 Views
  • 1 replies
  • 0 kudos

Nucleo running slower when externally powered

Posted on March 14, 2016 at 19:58HelloI am using a Nucleo-F103RB board (STM32F103RB) to read two ADC values every 1 second and display these values on an LCD.When the board is connected to the computer via the USB the ADC values are displayed every ...

ron_w by Associate III
  • 967 Views
  • 4 replies
  • 0 kudos

STM32F427 SDRAM Support

Posted on January 22, 2015 at 09:40We already have a product which uses an STM32F427ZIT: For our latest development we are in need of an external RAM. It would be great to control an SDRAM that hosts 128Mbit of memory (Organization 2M word x 16 Bit ...

karbach by Associate II
  • 2894 Views
  • 11 replies
  • 0 kudos

STM32L476 issue

Posted on February 09, 2016 at 23:18Hi,I'm trying to load demo SAI_audio-play from firmware package ''STM32Cube_FW_L4_V1.3.0''  into the flash but I can't, one error send me ==> Error: Flash Download failed  -  Target DLL has been cancelled.My setti...

0690X00000605ZtQAI.png 0690X00000605XUQAY.png 0690X00000605GtQAI.png

STM32F7 and LWIP issue

Posted on March 13, 2016 at 14:38I'm having issues with ethernet on the STM32F7 discovery and nucleo boards.I set up a simple Keil project using STMCube by using selecting the dev board when you create the project. I enabled ETH and LWIP and launche...

kalhana by Associate II
  • 1510 Views
  • 1 replies
  • 0 kudos

STM32F7 SAI/I2S slave issue?

Posted on March 09, 2016 at 13:53Hi, I am working on an application that streams audio from a WAV file on SD card. The core of the code is a hugely simplified version of the ''audio playback and record'' application from the Cube package. Audio outp...

USB cable connected

Posted on March 15, 2016 at 11:18Hi all, I'm working on a device with STM32F205. The MCU does to Stop mode after 15 sec. The device has also USB (VCP) and can be connected to PC. But I don't want MCU goes to Stop mode if USB cable is connected. So m...

donev_g by Associate II
  • 1248 Views
  • 1 replies
  • 0 kudos

Please fix errors in CubeMX FW

Posted on September 03, 2015 at 12:40In cmsis_os.c file -  osPoolDef_t pool_def = {queue_def->queue_sz, queue_def->item_sz}; + osPoolDef_t pool_def = {queue_def->queue_sz, queue_def->item_sz, NULL}; -     else if(ret.value.signals >= 0x80000000) + ...

vromanov by Associate II
  • 3122 Views
  • 6 replies
  • 0 kudos