STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC and DMA transfers for STM32F3.

Posted on April 26, 2016 at 05:17  Hi.I’m trying to get the DMA to transfer 10 data bytes from the ADC to memory (STM32F3.So far I can get this to work in ADCDMA circular mode, and this 10 sample conversion takes place continuously.I actually want t...

kvresto by Senior
  • 1181 Views
  • 2 replies
  • 0 kudos

Using AFE4404 with STM32F4Dsicovery

Posted on April 25, 2016 at 20:35 I have a question about using TI AFE4404 with STM32F4Disco. My question about power supply. I found in datasheet, that Supplies: Rx: 2 V to 3.6 V, Tx: 3 V to 5.25 V, IO: 1.8 V to 3.6 V And descripti...

DMA Interrupt

Posted on April 26, 2016 at 13:13 Hi I have a problem with the DMA Interrupt on a nucleo stm32f4 Everytime the Nucleo goes into an Infinite_Loop 1. .section .text.Default_Handler, ''ax'' ,%progbits 2. Default_Handler: 3. Infin...

STM32F7audio

Posted on April 15, 2016 at 11:48The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F405OE : Cannot connect with ST-Link

Posted on April 25, 2016 at 17:25Hi, We are experienced STM32 developers but we are having a real problem connecting to a new card, containing an STM32F405OE device. (the WLCSP 90 pin package). No matter what we have tried, the ST-LINK utility (v3....

execute code from RAM

Posted on April 25, 2016 at 16:26Hi My task is to execute a code from RAM instead of Flash but i dont know how can i able to do it . i am using f429 discovery.Could anyone help me ?Thanks 

arunl4g by Associate II
  • 2054 Views
  • 4 replies
  • 0 kudos

[STM32F746BG] Accessing internal Flash from code

Posted on April 24, 2016 at 18:54 Hi! I'm programming STM32F746BG using IAR 7.40 and J-Link debugger. I have a problem when trying to use internal flash to store some data. To be more specific when I try to erase sector 7. Here's my code: ...