cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F302xC is in wrong section in “stm32f3xx_hal_pcd_ex.c� file

thln47
Associate III
Posted on December 01, 2015 at 11:39

Hi, I use the STM32F3xx_HAL_Driver : Version V1.1.1 / 19-June-2015.

I use STM32F302RCT6 and STM32F303RCT6 devices and the USB device doesn’t work because the definitions of these MCU don’t match with the documentation ( RM0316 and RM0365).

Note: Info on RM0313 Rev4 page 807 table 105 is incomplete.

I’ve found some incorrect definitions on “stm32f3xx_hal_pcd_ex.c� file:

STM32F302xC is in wrong section, the MCU has the same USB_FS than STM32F303xC !

Line 148 :

#if defined(STM32F303xC)                         || \

    defined(STM32F303x8) || defined(STM32F334x8) || \

    defined(STM32F301x8)                         || \

    defined(STM32F373xC) || defined(STM32F378xx)

   

line 204:

#if defined(STM32F302xE) || defined(STM32F303xE) || \

    defined(STM32F302xC)                         || \           <---- wrong section for this MCU !

    defined(STM32F302x8)       

 

PCD_WritePMA, PCD_ReadPMA functions depend on access scheme type, so I decided to re-write these functions to select automatically the right access method. To identify this method, I write a known symbol on USB PMA buffer base address + 2.

On 1x16bits/word devices, this symbol can't be written and the read bytes are always set to zero.

On 2x16bits/word devices, the read bytes match with the symbol.

To optimize the access, I use DMA to transfer PMA buffer to (or from) the USB user buffer.

I attach the modified files with this post!
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
thln47
Associate III
Posted on December 08, 2015 at 14:34

The version V1.2.0 seems to be Ok