STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Don't working USART in STM32F051K8U6

Posted on May 30, 2016 at 21:58Hello. I'm use MCU STM32F051K8U6 for simple devices.I'm had a problem when using the UART.If i'm initialize USART thus (with SPL):It freezes the microcontroller, and the program is not executed.void GPIO_Initialization...

s9 by Associate II
  • 2408 Views
  • 5 replies
  • 0 kudos

Keil uvision debug script

Posted on May 12, 2014 at 14:19Hello,is there a possibility to make debuging scripts for STM32 processors in Keil uvision MDK? 

hospodar by Associate III
  • 1426 Views
  • 2 replies
  • 0 kudos

STM32L1 internal EEprom (user data in NVM)

Posted on May 29, 2016 at 23:18In STM32L1 how works the internal small EEPROM? (The Data EEPROM memory block. It contains user data)For example the Page 0 0x0800 0000 - 0x0800 00FF = 256 bytes, to use it must be first erased?For write is DATA_EEPROM...

Questions on what's happning before main() is called

Posted on June 01, 2016 at 16:19 I am working with the STM32F405/STM32F407 microcontrollers.I am trying to understand what's happening inside the microcontroller before main() is called and I would like to get rid of as much as possible to minim...

arnold_w by Senior II
  • 1776 Views
  • 4 replies
  • 0 kudos

Step+Dir Interface to STM32F4

Posted on May 30, 2016 at 05:42Hello, i am in the path of developing brush-less DC servo system for CNC mill, Because i will use motor encoder, as well as position quadrature encoder, i need ability of hardware tracking step and dir impulses. It wo...

HardFault at ORR instruction, what is happening?!?

Posted on June 02, 2016 at 00:28Hi,I am trying to get STM32CubeMX + arm-gcc + Nucleo-073RZ to do things. It won't.I can see in my debugger and lst file that08000990 <SystemInit>:SystemInit():/Users/dongfang/workspace-arm/stm32cube-playground/Nucleo0...

soren by Associate II
  • 1213 Views
  • 1 replies
  • 0 kudos

STM32F100C8T6B (Rev. Z) problem

Posted on June 01, 2016 at 16:35Hi all. I can't get more far than reset handler. On a first instruction I'm failing into HardFault_Handler. SCB->CFSR says  STKERR and IMPRECISERR.I see it only in STM32F100C8T6B. They all have rev. Z. All another chi...

STM32+HAL+SPI

Posted on June 01, 2016 at 17:01HiI'm trying to communicate with ADC through SPI interface with HAL layer and ended up with issues.At start I configure adc:HAL_SPI_Transmit(&hspi1, &SDATAC, 1, 3); //0x16HAL_GPIO_WritePin(GPIOC, START_Pin, GPIO_PIN_S...

0690X00000605OHQAY.png

STM32F429 USB Audio 16/24bit

Posted on March 21, 2016 at 07:51Hi, I want to ask you if it is possible using HAL to change usb format audio from 16bit to 24bit and vice versa. Now I can choose in windows between different frequencies of 16bit sampling, but if I change usb descri...