STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F439 RTC Problem

Posted on July 03, 2016 at 14:38Hello All,Micro-controller: STM32F439 With LSE(32.768 KHz)Standard Peripheral Driver Version: V1.6.1Problem: RTC routine StuckDescription:We are currently working on RTC and implemented the code as per available in st...

nipam by Associate
  • 2027 Views
  • 2 replies
  • 0 kudos

RTC time calculation in stop mode.

Posted on July 05, 2016 at 09:35 Hello, I'm trying to put my STM32F105 device into stop mode and it's important for me to keep calculating time. I'm trying to put system time into backup registers but then it somehow messes up my system. It seem...

marius1 by Associate
  • 2500 Views
  • 3 replies
  • 0 kudos

ST-LINK/V2

Posted on June 29, 2016 at 05:19In my systen, ST-LINK is working but in same environment ST-LINK/v2 is getting error. I am using STM32F utility for flashing my STM32F103ZET6, #too-vague

iftekhar by Associate
  • 1851 Views
  • 5 replies
  • 0 kudos

STM32F4 FMC on non-multiplexed SRAM

Posted on June 30, 2016 at 11:55Hi,I plan to build a board with an STM32F446VE + IS66WV51216EBLLAs the STM32F446VE is a 100pin package, it does not offer non-multiplexed interface on the FMC.So I was considering using the FMC in multiplexed PSRAM mo...

Kuikui by Associate III
  • 970 Views
  • 1 replies
  • 0 kudos

Losing timer compare interrupts

Posted on July 05, 2016 at 09:02 Hi, I try to setup two compare channels on TIM5 of a STM32F446 device to generate two independent time triggers. Both triggers have a frequency of approximately 8kHz but differ by a few timer ticks. Hence ...

how to config USB EP address instm32f407???

Posted on July 04, 2016 at 05:02In STM32F103,i use USB_EPnR to config endpoint address, e.g. I can config endpoint1 with adress 0x0a,so  endpoint1 can communicate with host endpoint10。 But in STM32F407 i don‘t find where to config endpoint adress,on...

wangsenme by Associate II
  • 1564 Views
  • 4 replies
  • 0 kudos

DMA starting and stoping

Posted on July 01, 2016 at 18:20Hi I use DMA for transferring data from ADC to ADCConverted[300] . I stop DMA somewhere in my program and get the position of the current transferred value by this command:  Current_Pos2= ((uint16_t)(DMA1_Channel1->CN...

STM32F303 Unique device ID - not BCD?

Posted on July 05, 2016 at 11:33Good day! I have a problem. In http://www.st.com/content/ccc/resource/technical/document/reference_manual/4a/19/6e/18/9d/92/43/32/DM00043574.pdf/files/DM00043574.pdf/jcr:content/translations/en.DM00043574.pdf said tha...

stmcufinder.com

Posted on June 27, 2016 at 17:07I stumbled upon http://stmcufinder.com today... interesting, appears to be genuinely ST-bred, but I don't remember to have seen a link to it anywhere on st.com. JW