STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART IDLE interrupt with DMA problem

Posted on September 11, 2016 at 06:59 Hello I have tried to use USART IDLE interrupt to align my buffer position in right address. #include < stm32f10x_gpio.h > #include < stm32f10x_rcc.h > #include < stm32f10x_usart.h > #include < st...

parisa by Senior
  • 810 Views
  • 0 replies
  • 0 kudos

V/F Converter

Posted on September 08, 2016 at 22:31Any Forum Discussions, App Notes or sample projects on using a micro to create a simple V/F converter? This isn't rocket science, but I do not want to reinvent the wheel either.

Keil514 error: #5: cannot open source file ''MCode.h''

Posted on September 09, 2016 at 00:45Hi guys,1. compile proj. Keil51 uVision: ->   error: #5: cannot open source file ''MCode.h'' 2. MCode.c   #include ''MCode.h''   ...3. Options for target -> c/c++ -> path ../user 4. user (MCode.h) etc.. Q: it see...

enmirc by Associate II
  • 1480 Views
  • 3 replies
  • 0 kudos

Run two motors in the same time

Posted on September 10, 2016 at 19:17 The main question is how to run two motors SecondMotorRotateToLeft() and FirstMotorRotateToLeft() in the same time? #include ''stm32f10x.h'' #include ''stm32f10x_gpio.h'' #include ''stm32f10x_r...

anton23 by Associate II
  • 787 Views
  • 1 replies
  • 0 kudos

STM32 F401 and HC-06

Posted on September 10, 2016 at 20:33Hi!I have problem with connection between my mobile phone and my Nucleo board by Bluetooth. How You see in subject I have a HC-06 and I can't connect with my mobile phone. When I try to do the same with my PC eve...

Read ADC Channel by Channel with hal

Posted on September 07, 2016 at 17:05hello every one.i want to run and use ADC on STM32f103.i can read the analog value from ADC_1 and channel_0 in single mode.but when i configure  ADC_1 and channel_0 ,channel_1 , channel_2 i can just read the anal...

l90mehdi by Associate II
  • 2962 Views
  • 5 replies
  • 0 kudos

Is this an ARM cortex-M4 based board?

Posted on September 10, 2016 at 06:56Hello I have bought this board about 3-4 year ago and didn't work with, and now I found it in my store and think this has stm32-f407-vgtb microcontroller on it, that I thought it's cortex-M3, but when I searched ...

STM32CubeMx FatFs & SDMMC ST32F7

Posted on September 10, 2016 at 12:37Hi every body.i configure STM32CubeMX to write on SD card. im using stm32f7 discovery board. i set SDMMC on ''SD 4bit wide bus''  and enabled FatFS for SD card.my main function is :int main(void){  /* USER CODE B...

Parallelism between CPU and FPU

Posted on September 09, 2016 at 22:14Hi.Is it possible to do some computation in parallel in CPU (with integers) and FPU (with floats)?Probably not, because both units need their own instructions to perform a math operation and the instructions can ...

matic by Associate III
  • 1121 Views
  • 1 replies
  • 0 kudos

External Nor Flash Programming from Application

Posted on April 16, 2013 at 16:40For my application I need to program external NOR flash via code executing on an STM32F4 family processor.  I see examples that read external flash but none that program it from code executing on an STM32F4 family pr...