STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4: Catch the last PC address before WD reset

Posted on September 20, 2016 at 11:20Hi all. I am trying to catch the last PC value before WD reset. For doing that I am configuring the WWDG and enabling its interrupt. then, while the WD interrupt fire I am writing the important information (i.e.,...

yonatan by Associate III
  • 3320 Views
  • 1 replies
  • 0 kudos

STM32F4 not fully programable

Posted on September 19, 2016 at 12:42Hello there, I have a problem with programming STM32F4 device. My Jlink probe correctly sees the device over SWD but it cannot erase nor program it however- This is the Jlink command prompt when trying to erase:h...

STM32F303 ADC Issue.

Posted on September 19, 2016 at 20:31I�m having difficulty getting the ADC to work on the F303 board in the the value returned is always 0.    The input line is PA0,  ADC1,  Chanel 1. The STM32cubeMX generated initialization code is as follows:   ...

markbell9 by Associate II
  • 1454 Views
  • 2 replies
  • 0 kudos

Port to low pin count MCU

Posted on September 11, 2016 at 08:17Hi, my apologies in advance for the newbie question.I have to port LCD sample program to 746VG(LQFP100) from 746NG-DISCO(BGA216).F746VG supposed to have a TFT-LCD controller, but I can't find LCD_R0/B1/B4 funtion...

yoshi by Associate II
  • 1343 Views
  • 2 replies
  • 0 kudos

STM32f205 + eMMC

Posted on April 19, 2013 at 17:20Hello,I try to interface a STM32f205 to a Toshiba eMMC via 8bit SDIO and DMA.In order to read and write can you please tell me if I am missing something:Read Single block Send CMD16 Block length (I receive the cor...

aoleon by Associate II
  • 1188 Views
  • 1 replies
  • 0 kudos

STM32F100RBT6B using timer TIM2

Posted on September 19, 2016 at 16:09 I have code that rotates small motor. #include ''stm32f10x.h'' #include ''stm32f10x_gpio.h'' #include ''stm32f10x_rcc.h'' #include ''stm32f10x_usart.h'' void Delay(unsigned int t) { unsigned int i...

anton23 by Associate II
  • 1080 Views
  • 1 replies
  • 0 kudos

Looking for SDIO+eMMC (not SD) example

Posted on February 03, 2012 at 09:20Hi , I'm looking for an example with SDIO+eMMC (and not SD). Is there something like that ? Another thing: Someone has information on eMMC commands ? Thanks Mikael #google #sdio+emmc-example

elharrar by Associate II
  • 5588 Views
  • 14 replies
  • 0 kudos

Compiling project error

Posted on September 10, 2016 at 14:54Hello. When I'm compiling a project genereted in CubeMX I've got this error: make: ***[Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal.o] Error 1. Do you know how to fix this?

michalt by Associate II
  • 1075 Views
  • 1 replies
  • 0 kudos