STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Where can I find libraries???

Posted on November 23, 2016 at 16:48Hi, I am new with the ST microcontroller and I was looking for some basic libraries. I am using a STM32F373CC and I want to use the SPI, ADC and DAC on the microcontroller... I have used the STM32 cube software to...

How to read Device ID Register in IDE

Posted on November 14, 2016 at 22:47I am using an STM32VLDISCOVERY with an accelerometer which is connected using SPI. I am trying to determine whether or not I have it connected to the STM correctly so I am trying to read its Device ID through the ...

Trying to make a USB HID mouse from cube mx

Posted on November 21, 2016 at 07:04 i have tryed to make working an usb hid mouse program (simulating mouse move) from cubemx: usb_otg_fs folowing youtube stm sample: https://www.youtube.com/watch?v=XRocqTfUxbo my platform is STM32F746DI...

0690X0000060MoOQAU.gif
lrou13 by Associate II
  • 1681 Views
  • 3 replies
  • 0 kudos

L4 LL drivers

Posted on October 12, 2016 at 19:06I'm confused about the development strategy.  Ideally, the Hal drivers should be layered on top of the LL drivers.  However, when I look at the code for say  gpio or spi, the Hal drivers duplicate the LL functional...

STM32F7 DISCO - memory sections

Posted on August 24, 2015 at 13:51Hi all,I have a question about the different memory sections. I use a modified version of the demonstration project.There are 4 memory sections:SRAMSDRAMFlashNOR (QSPI)This code save the variable to NOR:#if defined ...

benny by Associate II
  • 3867 Views
  • 10 replies
  • 0 kudos

System Tick timer is not incrementing uwtick

Posted on November 24, 2016 at 11:39 I have stm32F767zi nucleo, and I usedstm32CubeMXgenerate the code to test some of the functionality.The MX_CAN1_Init() returns Timeout error. I debugged HAL_CAN_Init(&hcan1) and found the section in the HAL_C...

x567234 by Associate
  • 1198 Views
  • 0 replies
  • 0 kudos

Connect DAC to subwoofer

Posted on November 17, 2016 at 15:51Hello I'm working on an audio system, I have stored audio files as binary data on an external EEPROM and using STM32F407VGT6 I'm taking this data and send it through DAC to external amplifier and then speaker. now...

DMA Weirdness

Posted on October 21, 2014 at 01:57Hello all,  I'm trying to run a ws2812 strip using a timer and DMA.  I'm using the stm32f303vct6 chip at 48MHz.  The Timer is running with no prescaler, and no clock division in PWM1 mode, with a period of 60 (1.25...

0690X00000605BXQAY.png 0690X00000605BiQAI.png 0690X000006057qQAA.png
arolsen by Associate II
  • 2796 Views
  • 6 replies
  • 0 kudos