STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

KalmanFilter C code error

Posted on December 30, 2016 at 12:04 I am using stm32f discovery board. I am trying to fuse Acceleromoter and gyroscope using KF. And here is a code i included that suppose to do this. #ifndef _Kalman_h #define _Kalman_h struct Kalman { /* Ka...

WIFI on STM32F

Posted on December 30, 2016 at 18:59looking at the STM32F103REY6 chip on the SPWF01SA, it has 3 SPI's. Are all 3 of these available to be programmed (I don't see them mentioned in the datasheet) or is it possible to use one of the SPI's MOSI/MISO,SC...

Resolved! Forcing static initialized arrays into FLASH (not in SRAM)

Posted on December 29, 2016 at 17:57THIS ISN'T A QUESTION - IS A RESULT.I was having issues getting some static arrays to stay in FLASH, not SRAM. Since they NEVER change, allowing them to load into SRAM just means the exist in both flash & SRAM (ak...

[BUG] FatFS + SDIO(DMA) L4

Posted on December 28, 2016 at 21:45Drivers supplied with CubeMX don't check if data that fatfs tries to write is properly aligned (32bit) this results in misaligned address send to DMA controller which is forced to be realigned and results in wrong...

ChrisH by Associate III
  • 999 Views
  • 2 replies
  • 0 kudos

Question regarding timer1 lib functions

Posted on December 30, 2016 at 00:28Hello,i am working on a BLDC motor control, based on hall sensors for rotor position.I am starting to write some code, and came across a example on googlethe function i am refering is this : TIM_SelectOCxM(TIM1, T...

Bogdan by Senior
  • 602 Views
  • 1 replies
  • 0 kudos

Problems with ADC interrupt

Posted on December 27, 2016 at 06:55 I am trying to generate an instantaneous PWM signal using ADC Single channel interrupt on stm32f103rbt6 nucleo board. I want to vary the speed of the dc motor using the instantaneous adc interrupt. But I am ge...

STM32F4 Ethernet not responding after power up

Posted on December 29, 2016 at 13:48We have a STM32F4 MCU on our boards, and recently have witnessed some strange behavior: The ethernet doesn't work after powering up the board. No pings, no TCP connections. After pressing the reset button on the b...

Maor Avni by Associate II
  • 1497 Views
  • 1 replies
  • 0 kudos

Code compiled as Release behaves different than Debug code

Posted on December 16, 2016 at 20:15Hello experts.Currently I experience a very strange problem with my firmware for a STM32F334.I just switched from the debug configuration to release, uploaded the code to the device and it behaves totally differen...

martin.k by Associate II
  • 3934 Views
  • 9 replies
  • 0 kudos

Does the STM32F103C8 have an I2C monitor feature?

Posted on December 26, 2016 at 15:27I want to implement a USB to I2C adapter.Since the STM32F103C8 has two I2C interfaces and a USB interface, it seems to be a suitable candidate.One of the features I'm looking for is a Monitor mode.Goal is to send ...

arno by Associate II
  • 2388 Views
  • 4 replies
  • 2 kudos