User Activity

Hi All, I need to design an PCB with STM32C011F6 (TSSOP20 package) that will have few inputs, few outputs and an ADC input (0V-3.3V).  I have seen the hardware design guide which talks about integrated oscillators of 48MHz and 32Khz but I'm not sure ...
Posted on August 18, 2016 at 12:01Hi All,I have two signal, one high signal having 20% duty cycle and a low signal with 40% duty cycle. High signal is  synchronized to low signal with reset trigger. I want to insert a delay of 100-400ns (t2 in diagr...
Posted on July 31, 2016 at 21:34The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on July 28, 2016 at 18:23 Hi All, I was trying to measure duty cycle and frequency of a pwm signal by using a timer with pwm output to generate pwm signal and another timer in reset mode to measure pwm using one of the example. Th...
Kudos given to