STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI problem in stm32f10x

Posted on January 06, 2017 at 17:40HelloHere is my code#include <stdio.h>#include <string.h>#include 'stm32f10x_gpio.h'#include 'stm32f10x_rcc.h'#include 'stm32f10x_usart.h'#include 'stm32f10x_spi.h'#define SPI_FLASH           SPI3#define SPI_CLK   ...

parisa by Senior
  • 1475 Views
  • 2 replies
  • 0 kudos

why uint8_t instead of char for strings?

Posted on January 06, 2017 at 12:42Why does the generated code from STM32CubeMX use uint8_t for strings, instead of the C standard char? The problem is that they differ in signedness, so gcc gives a warning. It's quite a pain, to be honest.I can see...

STM32F4 GPIO_ReadInputData while in AF mode?

Posted on January 09, 2017 at 21:35Hello,i have a bldc motor with hall sensors, each hall sensor is conected to PA0 PA1 PA2  which coresponds to CH1,2,3 of timer2.So in my gpio init routine i have declared the gpio's as followingGPIO_InitStructure.G...

Bogdan by Senior
  • 1519 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F7 EVAL Boot mode

Posted on December 06, 2016 at 02:50Hi,I am trying to put the STM32F769i_EVAL into system BOOT mode. I can do this successfully with an F429 Eval but not with the F7 Eval. I can see that when I reset it the normal program does not run , indicating t...

imtiaz by Associate II
  • 6912 Views
  • 16 replies
  • 0 kudos

STM32F030, stopping the IWDG

Posted on January 06, 2017 at 15:12We have a project that is required to go through UL testing, so it needs both a watchdog and a check that the processor frequency is running as expected. Because the independent watchdog uses its own oscillator it ...

STM32L0 96MHz mode or bad docs

Posted on October 07, 2016 at 02:39As a noob, I need to know whether there is a 96MHz mode as the documentation sugests====================================C:\Users\PD\STM32Cube\Repository\STM32Cube_FW_L0_V1.7.0\Drivers\STM32L0xx_HAL_Driver\Src\stm32...