STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Help for component identification

Posted on January 19, 2017 at 13:20Hi,I have this SMD component that I cannot identify:Package size: SMCMarking from top:<STMicroelectronics logo> (e3) GFBR GP 611I have no idea what this can be, and by the way, is there any place or list where one ...

F767 Nucleo RTC drift

Posted on January 15, 2017 at 09:01Hello,I have been using the RTC of the Nucleo 144 F767 board with the onboard 32768kHz oscillator and I noticed that there is a large drift (~2 minute lag per day or ~1570ppm).Based on the datasheet, the crystal dr...

STM32L476 I2C Reload bit

Posted on January 19, 2017 at 15:25Hi,I have a question regarding to L476 I2C architecture. In the datasheet, it asks to set RELOAD bit to one if Number of Byte(NBYTES) to transfer is larger than 255 bytes.In the reference manual, it's saying that I...

jiayuan by Associate II
  • 557 Views
  • 0 replies
  • 0 kudos

NRST Hardware Question

Posted on January 19, 2017 at 12:55Hey,I searched for this in the hardware development sheet but there was no real answer to my question. I do not want to use a switch at the NRST input, because i think everything what the switch does can be made wi...

luk by Associate II
  • 1397 Views
  • 2 replies
  • 0 kudos

NSS input not take into account on SPI SLAVE

Posted on January 18, 2017 at 10:47I have a system with 1 STM32F407 and 3 STM32F401. The 407 is the master  of a communication with SPI with the 3 slaves. On the slave a use SPI in slave mode with DMA in RX/TX. On the slaves the input NSS is used in...

New to external Sram Sdram

Posted on January 17, 2017 at 09:08Hello all We are new to external SRam and Sdram so I have some question we could don't verify the answer maybe because of language or lack of knowledge.we need to add external ram to stm32f4  and stm32f7So how to c...