STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F303K8 timer interrupt hangs

Posted on January 25, 2017 at 11:07Hi,I try to implement a timer with interrupt routine, but it always hangs after the timer is activated. This can be seen if I use the debugger over SWD: when I execute the next command after TIM_Cmd(TIM2, ENABLE); ...

4tschabos by Associate II
  • 1976 Views
  • 5 replies
  • 0 kudos

UART2 can't receive data from PC in STM32L476RG nucleo

Posted on January 24, 2017 at 11:54Hi allI'd like to use UART2 to receive data, but It seemed to be failed, only could transmitted data.I used the same codes in UART1, everything is fine,So I think HW and SW parts are fine except UART2.I had not con...

0690X00000605zpQAA.png

Resolved! STM32F4 GPIO functions

Posted on January 24, 2017 at 15:09I have looked at PM0214 Programming manual for STM32F4 series for functions like GPIO_Write() and GPIO_ToggleBits() but they don't seem to be there. Is there a document that describes peripheral functions or does o...

John Hite by Associate III
  • 1602 Views
  • 4 replies
  • 0 kudos

How to receive UART fixed length datas in sequence

Posted on January 24, 2017 at 15:27Hi allI'd like to use UART to receive soe fixed length datas, ex.'1234567890'.uint8_t buff[10]; hal_uart_receive_it(&huart, buff, 10); or hal_uart_receive_dma(&huart, buff, 10);How should I do and then make sure th...

CubeMx dma spi:Getting spi overrun

Posted on January 24, 2017 at 14:39Hi,I'm using latest version of Cube (download 20.01). I'm trying to read ADC-values from SPI with DMA. Read is activated on ADC-dataready.#define ADC_BLOCK_SIZE 24uint8_t tempBuf[ADC_BLOCK_SIZE ];// This interrupt ...

teijo by Associate II
  • 1470 Views
  • 1 replies
  • 0 kudos

F4 Analog Watchdog run-time reconfiguration?

Posted on January 23, 2017 at 18:35As the title says, can the analog watchdog high and low thresholds on F4xx be reconfigured while the ADC is running?I vaguely recall reading somewhere that it could be changed dynamically at any time but can't for ...

parsec by Associate III
  • 1647 Views
  • 2 replies
  • 1 kudos

CubeMX FreeRTOS USB and USB_CoreInit function

Posted on January 20, 2017 at 17:05HiI used STM32CubeMX and configured a project using RTOS and USB_DEVICE (I am trying to run the USB CDC functionality with the FreeRTOS). The program runs until it hits the USB_CoreInit function inside stm32f4xx_ha...