STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Master-Slave Interface STM32

Posted on February 04, 2017 at 16:52Hi All, I am trying to interface two STM32 discovery boards one as master and one as slave using the following code snippets. Sometimes the data seems to arrive correctly at other times it is corrupted. I just cal...

stm32f103 - minimize delay due to usart transfer

Posted on February 04, 2017 at 12:45Hello all,i am using a stm32f103c8t6 device, clocked at 72 MHZ,   the periph clock for adc is 12MHZ  ( 72/6).   Using  adc injected function with  sample time configured  at ADC_SampleTime_1Cycles5Timer 1 is gener...

0690X00000606FBQAY.png 0690X00000606DuQAI.png
Bogdan by Senior
  • 1863 Views
  • 4 replies
  • 0 kudos

Booting STM32F100 after flashing.

Posted on February 04, 2017 at 12:03I have built the simple led blink app using eclipse and gnu arm toolchain without any errors. I am accessing boot monitor via serial interface and programming the flash using stm32flash tool on linux, afterwards I...

STM32F072 PMBUS

Posted on January 21, 2017 at 14:10Hi,I have a STM32F072 in a board just like the Discovery F0.trying to get PMBUS upp and running with an external DCDC module.I can control it with waijung blockset in simulink sending i2c packets but now i need to ...

Resolved! STM32L452

Posted on January 24, 2017 at 13:20The Nucleo-64 UM1724 Rev.11 mentions STM32L452, but that's about all we know of this chip (one more ST presentation could be found on the net mentioning this model).As said UM is out for more than a year, is this g...

Resolved! STM32F437 clock problem.

Posted on February 03, 2017 at 19:44I have my clock setup for 168MHz and I see that with a scope at MD0. But a call to BSP_CPU_ClkFreq() indicates it is running at 550 MHz. This is the setup I have in bsp.c://  Configure for 8MHz XTAL => 168MHz SysC...

John Hite by Associate III
  • 1341 Views
  • 2 replies
  • 0 kudos

Resolved! DFU DFUSE problem with STM32L4 (STM32L476VG)

Posted on October 22, 2016 at 21:50Hello,We are implementing a product based on STM32L476VG and need to use DFUTo test the procedure we used  STM32L476VG Discovery board. The following issue has been found:- Compiled a simple LED switching applicati...

imalamoud by Associate II
  • 2386 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F407G-DISC1 read SD Card problems

Posted on February 03, 2017 at 13:38We have a problem using STM32F407G-DISC1.We have a custom PCB that mates with the DISC1 board. The PCB has an SD Card slot wired to SPI1 on the DISC1. We have tried a number of DISC1 boards about 50% of them are a...

Resolved! STM32L051 and VREF out

Posted on February 03, 2017 at 11:23Hello,I selected the STM32L051C6T6 for a small project (package LQFP32)The datasheet states that this microcontroller has a VREFint out pin (PB1, additionnal functions).I just can't find out how to output the inte...