STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030 ADC in DMA mode blocking other HAL functions

Posted on February 07, 2017 at 20:27Hi all,I have configured ADC to work in DMA mode for 4 channels. Code was generated via Cube. After I call function HAL_ADC_Start_DMA everything works fine until I trying to call other HAL function. In this case, ...

Piotr Rog by Associate II
  • 5000 Views
  • 9 replies
  • 0 kudos

Heap size

Posted on January 11, 2017 at 11:32Hi,I'm working with a stm32f437VI. I need more heap memory. I changed the Heap size in de startup_stm32f427x.s (Heap_Size       EQU     0x00000200), but when I did a malloc and worked with the variable, and excepti...

cricart by Associate II
  • 3433 Views
  • 7 replies
  • 0 kudos

How to send additional bit?

Posted on February 06, 2017 at 18:09Hello,I'm trying to implement a software that will allow me to send additional one pulse (on the data wire and clock wire). After one pulse I should send data (32 bits) over spi.Frame should look like:1 bit + 32 b...

John Doe1 by Associate III
  • 4200 Views
  • 12 replies
  • 0 kudos

FlashLoader demonstrator for STM32L031G6

Posted on February 09, 2017 at 11:00Hi I need a target file (*.STmap) for downloading the STM32L031G6 using the 'Flash Loader Demonstrator' V2.8.0. I only got STM32L0_x3_x2_x1_64K.STmap, but STM32L031G6 is only 32K.

STM32F405 I2C lock if one clk pulse gets lost

Posted on February 08, 2017 at 13:19If the master sends the adress , but doesn't send the last clk pulse to receive the ACK from the slave, the slave will not release the SDA line. The problem is, that the ADDR-Flag only gets set AFTER the ACK was s...

0690X00000605JNQAY.png 0690X000006068hQAA.png

STM32F4 DMA interrupt not generated all the time

Posted on January 27, 2017 at 11:16Hello All,I am using STM32F407 discovery board. I am using SD IO card with this board.I tried configuring DMA for data transfer.I observed that the interrupt (DMA interrupts) are not generated after Transfer comple...

STM32F429i-DISCO with 512Mbx16b memory

Posted on February 06, 2017 at 12:34Hello, in my project i need to have more SDRAM than original 4M*16b.So i ordered 32M x 16b ISSI IS42S16320d-7TL that fit's inside the same footprint, and i soldered single jumper cable to PG2 as well as modified G...

Using TLC2543 ADC chip on STM32L476RG

Posted on February 08, 2017 at 11:33Hi allI followed the post below to setup tlc2543.http://blog.csdn.net/haozi_1989/article/details/6111776 datasheet http://www.ti.com/lit/ds/symlink/tlc2543-ep.pdf Because the STM32L4 series used HAL library not SP...