cancel
Showing results for 
Search instead for 
Did you mean: 

Low-layer in STM32F0

clsilva78
Associate
Posted on September 14, 2016 at 20:24

I want to develop an application using low-layer drivers in keil ide / stm32f051x. I can't compile because some funcions of sm32f0xx_ll_rcc the compiler says ''implicit declaration of ..''

I ca compile de example provided in  the stm32cubef0, but if I change the uC to another I cant compile.

I change the preporcesor simbols, asm file, etc...

Any suggestions

Thx por your Attention
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on September 16, 2016 at 16:06

Hi csilva,

I ca compile de example provided in  the stm32cubef0, but if I change the uC to another I cant compile.

1-Which example did you looked to?

2-What are you using as STM32 product?

3-Could you please provide more explanation on your case, so that it will be easier to understand the issue?

-Syrine-