STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I cannot find GPIO_PinAFConfig function

Posted on February 22, 2017 at 06:02I am using visualgdb.com tutorial 'Using STM32 timers in PWM mode. It has a function calls 'GPIO_PinAFConfig' as well as 'TIM_OC1Init' but I cannot find it in any of the headers.

STM32F7 - Power Fault

Posted on October 01, 2016 at 08:57I am working on connecting a ESP8266-01 WiFi chip to the STM32F769NI-DISCO board. I have enabled UART5 in STM32CUBE and put EXT_SCL, EXT_RST and EXT_SDA into high impedance mode by putting them as inputs with NOPUL...

USb OTG FS Device Mode with STM32F412/411

Posted on February 09, 2017 at 03:07Hi all,I am currently trying to get USB OTG FS working with STM32F412/411 MCUs in device mode but unfortunately the PC doesn't recognize the device. Cannot figure out if it is a hardware or software problem becaus...

STM32 Flash Driver Not Available from STM32CubeMX

Posted on February 21, 2017 at 17:40Hi, I want to port a IAP CubeMx project for the STM32091C_EVAL board (https://github.com/borgel/STM32Cube-F0-Releases/tree/master/Projects/STM32091C_EVAL/Applications/IAP) to a custom board using the STM32F0CB. I ...

Touchscreen setting on custom board (STM32F7 MCU)

Posted on February 17, 2017 at 15:37Hi, I have a custom board based on the STM32F769IBIT MCU. I want to implement a BSP layer as there are with ST discovery boards. I've already implemented the SDRAM, the flash and the LCD (densitron 84-0226-000T) b...

enia ami by Associate II
  • 4769 Views
  • 4 replies
  • 0 kudos

STM32f072 can bus crytal-less possible?

Posted on February 21, 2017 at 11:04Hello forum,I am planning to design a new module for my can-bus based home automation system (https://github.com/klaus-liebler/sensact ) with a STM32F072. The CAN bitrate ist 125kbps. It would be great if I could ...

KLausL by Associate II
  • 3738 Views
  • 3 replies
  • 0 kudos

CubeMx code generation hangs

Posted on February 18, 2017 at 08:30I am using 100 pin, STM32L4 mcu. After i updated to cubemx 4.19.0 a few days before, it takes more time to generate code for larger projects (more peripherals), which goes upto approx. 3 to 4 minutes. For smaller ...

STMF0x + CANbx + HSI48?

Posted on February 21, 2017 at 01:01Hi, My using the STM32F072 with CANBus. I was going to use the HSI48 throughout however I discovered an issue.  According to the Bosch CAN specification...'A maximum oscillator tolerance of 1.58% is given and ther...