STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with ADC Dualmode with 12 bit and DMA

Posted on February 23, 2017 at 16:58Hello, I am using the stm32f334 and try to use both adc in dual mode with 12 bit and one dma channel. With 8 bit halfword everything works fine. But when i use 12bit and DMA set to WORD array and HAL_ADC_GETVALUE ...

WIFI HTTP POST issue for JSON data

Posted on February 23, 2017 at 13:39Hello, I am using STM wifi module to transmit data to server and the data is in JSON format. for transmitting data i am using HTTPPOST method. e.g. AT+S.HTTPPOST=requestb.in,/16oftr91,{'Data':'12345'}Data is succe...

sandeep by Associate
  • 1008 Views
  • 0 replies
  • 0 kudos

STM32F769I-DISCO noise

Posted on June 19, 2016 at 01:46 Hi, I want to ask if someone can confirm that the STM32F769I-DISCO has a high-pitched https://www.dict.cc/englisch-deutsch/buzzing.html https://www.dict.cc/englisch-deutsch/sound.html. I think it's from th...

benny by Associate II
  • 6599 Views
  • 23 replies
  • 0 kudos

Setting BFB2 in field possibly bricking OPTCR ?

Posted on February 23, 2017 at 13:06Dear Forum, I implemented a in-application update similar to AN4767 with an STM32F429 CPUMy current problem is the short amount of time ( approx 200ms ) while programming the optcr register to set the BFB2 bit.As ...

stst9180 by Associate III
  • 683 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F72 and STM32F73 reference manual?

Posted on February 19, 2017 at 09:48I'm wondering where to find reference manual for STM32F72 and STM32F73 chips? I was able to find the datasheets - directly from the site of the particular chip - but the reference manual is not available from the ...

Define interrupt handler as weak

Posted on February 22, 2017 at 10:31I need to define my own interrupt handler. Cube not not generate the ISR as weak so everytime I regenerate the code with cube, I have to modify the code to hide the interrupt handler generated by cube.Would it be ...

Adalgiso by Associate II
  • 2919 Views
  • 4 replies
  • 0 kudos

trace error in stm32f411 Discovery Board in true studio

Posted on February 23, 2017 at 07:52Hi,I have configured stm32f411 I/O & clock & etc. in STM32CubeMXand generated source code in true studio.After that, I have connected stm32f411 discovery board and started debug in true studio.Then when I trace by...