STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The problem with ethernet on STM32F407

Posted on April 06, 2017 at 23:50Hi all!I want to study the ethernet on STM32F407!I have the working board with lan8720, stm32f407 and LEDI connected this board to PC through Ethernet cable/First, I want to know,,that frames from PC are written to R...

Hard Fault When I enable the USART3_8_IRQn interrupt.

Posted on April 18, 2017 at 23:07Hi Forum,I'm using the stm32f091, but when I enable the USART3 interrupt, the system hard faults. I already use USARTS1 and 2 without any problem. Not sure what else is required, so I'd be grateful for some assistanc...

stenasc by Senior
  • 2301 Views
  • 5 replies
  • 0 kudos

Problem with WiFi shield FW

Posted on April 18, 2017 at 21:11Hello everyone,I have a problem with wifi shield.I followed the 'WiFi-en.DM002450122 'manual (first file) to move the UART1 from PA9 and PA10 to PB6 and PB7 (removing \ shifting resistors), now I have tried to downl...

STM32L432KBUx can't load program

Posted on April 19, 2017 at 12:00Hi there ,We using AC6 IDE to develop our application based on VL53L0X and STM32L432KBUx. Everything was good until I can't program my target.At the beginning only the debug session worked fine. But now I'm not able ...

STM32f030cct6 port pin failure

Posted on April 18, 2017 at 12:47we developed thermal printer solution using STM32F030CCT6 controller.The issue after 3 or 4 days of working on end user's site some of the pins failed (i mean showing zero resistance to ground).scenario is as below.t...

karan by Associate III
  • 2571 Views
  • 5 replies
  • 0 kudos

Problem to download from ST Link of EWARM

Posted on April 16, 2017 at 13:45Hello! I can't download to STM32F103C8T6 via ST-Link(ST-Link V2#) of EWARM.The error message is attached.Please let me know your comment.

L C by Associate II
  • 2934 Views
  • 6 replies
  • 0 kudos

How do I do a DSI Read?

Posted on April 19, 2017 at 03:53All of the examples in the Cube only write.  There is no example code for a DSI Read. And I'm obviously not understanding something because the commands in the hal driver dont jive with the data sheet for the otm8009...

TIM15 does not outpu pulses in OPM mode

Posted on April 18, 2017 at 15:17I tried STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\TIM\OnePulse examples after adding systick timer to generate 50Hz square wave looped back to timer input. This was easiest way to test it. I...

fshah48 by Associate II
  • 3303 Views
  • 7 replies
  • 0 kudos