STM32F4 Bad UART communication
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-11-13 7:00 AM
Posted on November 13, 2016 at 16:00
Hello,
I created a project using CubeMX and I want to send messages via UART. I used a HAL_DAC_Start_DMA function. My problem is that when I'm sending some messages only 20 first characters are sent but after I send some another messages those wrong ones works fine. Also I noticed that only for optimalization level: Optimize for size UART transmission works.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-11-13 7:11 AM
Posted on November 13, 2016 at 16:11
Do you think your presentation is adequate to understand what your code is doing?
Tips, Buy me a coffee, or three.. PayPal Venmo
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
‎2016-11-13 7:24 AM
Posted on November 13, 2016 at 16:24
For example:
I'm sending to uC command SET_FREQ 100\r and uC should send message OK FREQ SET TO 100Hz\r\n but i receive only OK FREQ SET TO 100. But then I send to uC command SET_SIGNAL SINE\r and uC send message OK SIGNAL SET TO SINE\r\n as it should. And then I send command SET_FREQ 100\r and uC send full messege OK FREQ SET TO 100Hz\r\n.