STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS25HB usage with Cube HAL Library

Posted on April 30, 2017 at 06:36I am having significant difficulty in getting an LPS25HB to work. Temperature and pressure values returned by the sensor are incorrect. And although the sensor is sending the MSByte first, as expected, it is sending ...

STM32L151 clock issue

Posted on May 01, 2017 at 09:11Hi,i am using STM32L151 in our borad and for main clock source i have used pericom 8mHZ crstal and when i am trying to observe clock on scope ,i am unable see the clock.But SW team programmed the controller and with LE...

Stop mode with Interrup EXTI

Posted on April 28, 2017 at 10:17Hello family ST,I would like to use stop mode with an interrupt Pin,I tried the PWR Stop example in STM32Cube_FW_L0,When I put the PA12 Pin to Vcc I have ?c wake up after it runs the program and so it resumes stop mo...

ibrahim by Associate II
  • 1439 Views
  • 2 replies
  • 0 kudos

udp packet sender

Posted on May 01, 2017 at 15:08I've implemented on my board the UDP packet server as a task for a board which has to support ethernet, but nothing is defined for the interface.  So far so good.  I send UDP packets to it and it receives and echoes th...

SPI questions

Posted on November 27, 2016 at 23:40I'm using F3 and L4 processors and have a few spi questions1)  In half-duplex mode, how do you receive a single byte with a master ?  two bytes ?  It appears from reading that in this case, the SPI clock runs as l...