STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Return value from CMSIS osSemaphoreWait

Posted on December 17, 2015 at 10:40 According to the http://www.keil.com/pack/doc/CMSIS/RTOS/html/group___c_m_s_i_s___r_t_o_s___semaphore_mgmt.html#gacc15b0fc8ce1167fe43da33042e62098(CMSIS version 1.02) the return value should be the number ...

soren2 by Associate
  • 1885 Views
  • 2 replies
  • 0 kudos

STM32F042 Nucleo USB detect connection and disconnection

Posted on September 02, 2017 at 14:55Hi all,i have a problem with STM32F042 Nucleo and USB Connect detection.I made my own MIDI Interface with CUBEMX (generated a CDC Projekt and changed it with help from some internet sites to MIDI) and it works we...

hans23 by Associate II
  • 3041 Views
  • 5 replies
  • 0 kudos

STM32Cube_FW_L4_V1.8.0\Projects\STM32L432KC-Nucleo\Examples\PWR\PWR_STANDBY_RTC example project

Posted on September 01, 2017 at 19:36Hi I just purchased the STM32L432 Nucleo board  and tried to run the example from the folderSTM32Cube_FW_L4_V1.8.0\Projects\STM32L432KC-Nucleo\Examples\PWR\PWR_STANDBY_RTCI found that I could not find the definit...

Resolved! STM32F4xx_StdPeriph_Templates missing file

Posted on September 05, 2017 at 16:11Dear All,Currently I've just got a STM32F429ZIT6 Discovery kit from ST.Q1. I'd like to exam the simple gpio firmware into my kit. So I open the STM32F4xx_StdPeriph_Templates  project in Keil. But I come across th...

0690X000006044VQAQ.jpg

Resolved! Why does STM32F4 Discovery kit

Posted on September 05, 2017 at 14:03Hi,I've just got a STM32F4 Discovery kit (STM32F429)I thought that it embedded software for demonstate at the first time.But my kit does not work.I also I read the below instruction.But I don't know should I have...

STM32H7 maximum sdram frequency

Posted on September 05, 2017 at 10:37The STM32H7 series drive SDRAM by fmc,Which is maximum sdram frequency 100Mhz or 200Mhz can run?There are four input clock sources for fmc_ker_ck, and SDRAM clock can be fmc_ker_ck/2 or fmc_ker_ck/3.If I choose c...

0690X000006087sQAA.png
HAN Wu by Associate
  • 3037 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX: Problems installing new libraries

Posted on February 13, 2017 at 11:52I am using STM32CubeMX Version 4.16.1 on a pc without(!!!) internet access.I would like to install a new library via 'Menu'/'Help'/'Install New Libraries'/'From Local...'.I have downloaded the firmware package for...

Tob G by Associate II
  • 3505 Views
  • 6 replies
  • 0 kudos

STM32F7 dual bank random RWW stalls

Posted on June 28, 2017 at 11:13Hello everyone,I am having very weird problem using RWW functionality on STM32F767VIT6. I have searched through various places and found no hints to my issue. Any pointers are welcome.My flash organization is followin...

how should i handle httpd_cgi_handler()?

Posted on September 05, 2017 at 16:58Hi there!new LwIP stack given by STM32Cube calls httpd_cgi_handler() from httpd.c file. Unfortunately i could not find any docs or examples on how to use this hande (i.e. how to make my own CGI processing).Any he...