STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SW4STM32 and C++

Posted on October 23, 2017 at 00:32Hi Everyone.I mostly work with a C environment when I create a STM32 project but in the last few days I have been creating STM32 C++ projects by selecting a C++ project instead of a C project, and I can see in the ...

mbmail4 by Associate II
  • 1328 Views
  • 2 replies
  • 0 kudos

Is it dead? FAIL.TXT

Posted on October 23, 2017 at 21:37Excited getting the STM32L476 Nucleo-64 board from the ST event last week. Was trying to program it past few days. Tried some examples from mbed with IDW01M1 WiFi module. But it was iffy, at times program just hang...

Timer2 channel 3+ADC+DMA

Posted on October 20, 2017 at 22:51Hi    I am using STM32L431xx Timer3 and CC3 (compare mode ) on channel 3 and i want to trigger (ADC1  channel 1) and (DMA 1 and channel 1 ) to do collection of samples triggered on the timer edge. The timer works p...

STM32F107 PA15

Posted on October 23, 2017 at 13:47I'm not able to turn high PA15 output.All other pins (PB2, PB3 etc) correctly changes output with GPIO_SetBits/ResetBits.I'm using Keil and SWD connected programmer.I've checked with oscillator output but it's all ...

STM32F042 usb device fails

Posted on October 20, 2017 at 18:51Hi, I'm attempting to make a usb audio device using an stm32f042. I have managed to prototype the same basic concept using an F4 discovery, but the same code (with some changes and new CubeMX autogenerated parts) f...

Usage Fault PSP=0x00000020

Posted on October 22, 2017 at 11:18Hello,I have a project with an STM32F446, with RTX, 3 threads (main + 2 declared by me) + of course the idle one. The main thread enters wait state after starting the two threads so i have just two threads running....

andrei by Associate II
  • 1686 Views
  • 2 replies
  • 0 kudos

How to have a good precision of ADC on STM32F103C8?

Posted on October 23, 2017 at 05:58Hi.Now I'm trying to implement the ADC on the STM32F103C8.but I came across some problem when I voltage leveling test.The code is here  x = getPot()*3.3/4095; //get analog value and convert to volts, 12bit ADC if(x...

0690X00000608eNQAQ.png